12-04-2015
08:07 AM
- last edited
a week ago
by
AmyReyes
Hallo Zusammen,
die Installation hat nun reibungslos funktioniert. Nur kann ich das Programm nicht nutzen, weil beim Erstellen oder Öffnen einer Datei das Programm abstürzt. (Fehlermeldung siehe Screenshot)
Konfiguration: Windows 10 home auf einem Lenovo Thinkpad SL510
Kann mir jemand weiterhelfen.
Gruß
dtpchris
12-04-2015 11:38 AM
Hi @dtpchris
Sorry you're having problems with this installation. ST6 was released some years before Windows 10, so my first recommendation would be to install ST8. Is that an option?
Thanks
Melanie
12-07-2015 02:55 AM - edited 12-07-2015 03:02 AM
12-07-2015 05:13 AM
Hi there @dtpchris,
Yes, the ST8 version has been available for a while now.....highly recommend upgrading.
I have installed Solid Edge ST8 Student Edition, and it is running on my daughters lower spec Windows 10 laptop, with no issues.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000
12-07-2015 07:52 AM
hi @SeanCresswell,
i already uninstalled the st6 verion.
is there any download link for the st8 student version?
thanks
dtpchris
12-07-2015 09:43 AM
Hi @dtpchris
The download link is here:
You will need to re-register for the upgrade, and the actual download link will be emailed to you.
Thanks
Melanie