Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter

When i insert my Academic Code in the blank, this happens:

 

solid edge.png

 

The "Ok" button do not change to available. What should i do?

 

--- This is the STUDENT VERSION ---

21 REPLIES 21

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter
 

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

You mean ST6....as there isn't an download for ST7 Student Edition yet.

 

Probably the key you have placed there is either incomplete, or contains excess characters...copied not enough, or too much from the email text.

 

The "OK" button should be active when the license string matches the criteria. [I don't recall what one looks like, so don't recall if there are spaces, dashes, etc...]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter

But the program is ST7 student version, this image is a previous installation because in this moment I have installed ST6, but the license code in ST7 not working.

 

I feel the same as the person of another review

 

Sin título.png

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter

With the opcion "I have a license file"  and entering license file of ST6, it actived ST7

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter
In my case is doesn't work men

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter

No, i mean ST7 !

See the icon:

st7ico.png

 

and this problem is happenng also: 

errost7.png

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter
Yeah, in ST6 the license ran normally, but in ST7 not work.

playing wait

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@davidjaramillo9 wrote:

But the program is ST7 student version, this image is a previous installation because in this moment I have installed ST6, but the license code in ST7 not working.

 

I feel the same as the person of another review

 

Sin título.png


 

Well that is news to me! [not that I'm expecting to be kept in the loop by the Seimens crew].....I'm pretty sure there is a "University Edition", which I believe requires an site specific license file, similar to the commercial version. Is this what you have access to?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge ST7 Activativation using Academic Code is not working!

Experimenter
Experimenter
I undesrtand, but my version is Student , and required a Academic Code.. then , when i install the product and i will activate, appears the same problem of the first comment