Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 - Maintenance Pack 1 Announcement

Siemens Legend Siemens Legend
Siemens Legend

September 26, 2014

 

 

Dear Solid Edge Customer:

 

Solid Edge ST7 Maintenance Pack 1 for Solid Edge is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.

 

In order to deliver the first ST7 Maintenance Pack in a timely manner, ST7 Maintenance Packs will continue to

be delivered using RTPatch technology and will require a complete uninstall of Solid Edge in the event a ST7 MP

needs to be removed.

 

================

Download Location:

================

 

ST7 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST7/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 7175283: Fixed length key point curve API does not work when curve goes thru key points

 

===Assembly===

PR 1994198: Impossible to select component in frame application

PR 7171757: Pipe component (axis) is not aligned with 3D sketch element on edit of Pipe Rout

PR 7173742: Enclosure does not update after moving parent component

PR 7173809: Assembly Feature does not update after Drag Comp

PR 7174425: Solve behavior changed for some assembly connect relationships

PR 7175178: Crash in assembly frame environment when SSD file is renamed

PR 7177852: Lower PathFinder shows Assembly Feature driving part file

PR 7178804: Need to support NX 10 created JT files

PR 1984803: Failed assembly relationships when opening some alternate assembly files

PR 7181086: Placing adjustable part in assembly crashes Solid Edge

PR 7183520: Hidden reference planes display when they shouldn't

PR 7187374: Crash when duplicating an adjustable assembly

PR 7187548: Abort when certain patterns are edited

PR 7189285: Fence selection performance issue with Steering Wheel enabled in large assemblies

 

===Draft===

PR 1989738: deleting a detailed drawing view leads to a crash

PR 1993512: Grid origin moves when opening previous version file.

PR 7174232: Edit Links change source was disabled if the linked document was not loaded

PR 7176351: Alt moving coordinate dimension not working with dimensions in both directions

PR 7177052: Lock dimension button is no longer disabled after selecting edge

PR 7175214: Coordinate dimensions cannot be aligned in this case

PR 7178804: Filled fonts" polyline representation not supported on import

PR 7185254: Cannot disconnect leader if attached to callout (preserves associativity)

PR 1986615: Cannot delete link from draft file

PR 1996610: Dimension Style with ',' will not be exported to DXF

PR 1997629: Certain Files crash ST7

PR 7190079: Copying views that have display depth specified

PR 7192924: DECs don't show up for rectangle sketch elements when using hot keys

 

===Part/Profile/Sheet Metal===

PR 1844241: Synchronous edit succeeds only with smaller modifications

PR 1991815: Flat Pattern fails, if using DIN.PZL instead of Standard Formula

PR 1992122: Cannot create a Flat Pattern of a Family of Part members created in Part

PR 1994161: Database for Holes does not work with Open Office as the standard program

PR 7143560: Can't create a ruled surface on my part

PR 7159816: Importing specific Catia V4 file in ST7 is slower than ST6

PR 7167802: Thread button is selectable when editing holes with not-found DB

PR 7171794: Regions are getting created from the protrusion faces having 3D sketch in it

PR 7172172: Invalid DB file allows selection of hole types

PR 7173598: Abort when in Etch command and select text profile then Pan the view and RMB

PR 7173696: Cannot place feature library first time after viewing simulation results

PR 7173728: Orientation plane is skewed when locking to plane during hole placement

PR 7174023: Measurement line not displayed in this workflow

PR 7174072: Style Organizer shows wrong file and always defaults back to that file if change

PR 7174099: Dimension text doesn't print

PR 7174567: Flat Pattern cmd QB displayed partially after view manipulation cmd is executed

PR 7175074: User not prompted to save on closing after pasting FEA elements

PR 7176003: 3d sketch responds slowly while drawing especially when other geometry

PR 7176505: Using the scroll wheel causes values to go to beginning of range instead of next

PR 7174824: Profile region performance issue

PR 7185374: Tapered external pipe threads fail to apply correctly

PR 7185661: Thread length incorrect when placed using system selection

 

===Mold Tooling===

PR 7169079: Abort when creating runner bars on one side only

 

===Insight===

PR 1984313: "Free Text" search problem with option "Search for results in subfolders"

PR 7142238: Insight: Revisions issue with LCA & Revise operations losing revision history

PR 7181475: Error in saving any new file to Insight Server in ST7

 

===Insight Connect===

PR 1990745: Standalone Solid Edge Viewer doesn't open all parts

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7167082: Save As action saves psm to an already existing prt and overwrites its dft.

PR 7168085: Can't access RMB menu in new web browser session

PR 7169528: dwg and .pdf files not uploaded to location defined by SESP URL property

PR 7169551: For some folders, objects are not getting populated in delete dialog

PR 7173862: Save As All in Structure Editor generates different sequence numbers

PR 7176714: Workflows get stuck when an object is checked out

PR 7177270: Synchronize command fails with UAC enabled

PR 7177731: Cannot populate Look In field on Search dialog from Add to PCF

PR 7183870: Upgrade from ST6 to ST7, STD parts doc lib seen under wrong site

 

===Solid Edge Embedded Client===

PR 1992713: Add To Teamcenter Interactive incorrect Item ID when using display names

PR 1992719: SESE not using Naming Rules on Item Id and Item Name correctly

PR 6986382: MRU shows wrong preview when mutliple revisions are in the MRU

PR 7110098: Save As- User gets file load failure using this workflow

PR 7133799: CPD Ctrl-V paste does not keep values if the user double clicks the field first

PR 7157794: SEEC CPD - Save Copy As on an item with a drawing, gives a different part number

PR 7168042: SEEC Diagnostic: "TEAMCENTER DATABASE LIST" is not populated

PR 7168075: SEEC Diagnostics: Info is missing from log if FMS can't start

PR 7168465: MT9_Drawing item type naming rule patterns for ID and revision are ignored

PR 7168981: Unable to perform action if dataset having broken XLS link for this test case

PR 7170830: Insert Part Copy behaves differently in Solid Edge managed vs. unmanaged

PR 7174699: Asian characters in TAL log for English system

PR 7175353: Remove All on the Project ID will not remove the Project ID for model and draft

PR 7176006: The Insert Weldment link is shown as a red question mark

PR 1991572: Problem setting SEEC_ItemTypeList_SE Part and SEEC_ItemTypeList_SE Draft

PR 7169854: Item Name in Solid Edge CPD not synchronizing between Part and Draft file

PR 7182263: Mapped date property is converted to a custom text property via SaveAS

PR 1993092: BOM mismatch with Save As Copy of read-only Precise IPA'ed assembly structure

PR 7176282: Crash observed while repairing broken link

PR 7181609: Preview Image on Cache Assistant dialog is distorted as width is increased

PR 7182797: Save As of draft with Asm does not update Asm dataset name with revision

PR 7189106: Save as fails for this specific Teamcenter Item revision

PR 7118226: Import Template reports Success if FMS not configured correctly

PR 7168059: Open as read-only setting uses stale data

Regards,
Fred White
Siemens PLM Software
24 REPLIES

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Experimenter
Experimenter

1. Please, document officially how to deploy ST7 MP1 silently. Setup.exe /s does not seem to work now? It is important generally for the updates to be automated /and controlled/. 

2. Are you planning to develop or use some better update technology? MSP files, auto update within the program (like Autodesk), etc.?

 

I hope that as SolidEdge is being improved in some areas like Synchronous Technology, other areas like updating, options deployment (without need of user interaction) for multiple users will be improved as well. 

 

Regards,

 

Mesru

 

 

 

 

Highlighted

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Gears Phenom Gears Phenom
Gears Phenom

ST7MP1.png

What's wrong??

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Phenom
Phenom
I believe you try to install the share point maintenance pack instead of the Solid Edge maintenance pack.

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Gears Phenom Gears Phenom
Gears Phenom

The file is in the screenshot.

Why oh why is this prehistoric update system still in use...

 

Even free software has a "check for update" button which starts the correct update process after one click. 

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Phenom
Phenom
The Solid Edge ST7 maintenance pack file is called:

Solid_Edge_MP1.exe

the file you have downloaded is for the Share Point client.

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Indeed, I looked over it. Thanks

 

Nevertheless, I still don't understand this kind of work...

 

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Phenom
Phenom
Built in update system and maintenance uninstall should be implemented for a better user experience.

Is it time for an enhancement request ?

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Mesru,

you have to unpack the provided ...MP1.exe file.

(I am using 7zip software to do this).

 

After unpackicg, there is a bunch of files. I use this script for silent install of MP

It works for ST6, not tested on MP1 for ST7, but I pressume that there will be no changes in MP install package.

 

Script:

"%folder%MP\MP10\SE64MP10\setup.exe" -s -f2C:\temp\ST6MPXXsilentsetup.log

 

Hope this helps.

 

Ota

Re: Solid Edge ST7 - Maintenance Pack 1 Announcement

Gears Phenom Gears Phenom
Gears Phenom

I had no crashes until MP1.

Already 5 since yesterday.

 

Am I the only one?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user