Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 - Maintenance Pack 10 Announcement

Siemens Legend Siemens Legend
Siemens Legend

October 5, 2015



Dear Solid Edge Customer:


Solid Edge ST7 Maintenance Pack 10 for Solid Edge is available for download.



The Solid Edge Team




Release Notes:



Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.



Download Location:



ST7 Maintenance Packs can be downloaded from:






There were Solid Edge Embedded Client policy file updates in MP2. It’s vitally important that you install SEEC

Administrator, which delivers the policy files to TC_DATA.


Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.


Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.



E-mail Notification:



To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.


To initiate your subscription, navigate to: for the web interface.



This Maintenance Pack addresses the following PRs:




PR 7467945: Need a method to kill a command from the BeforeCommandRun event



PR 1989085: Setting subassembly as adjustable and assemble it cause that patterned parts be

PR 7383011: femap running in background, locking up my assembly

PR 7478836: Solid Edge Physical Properties not matching results from API

PR 7453978: Hole Feature recompute Fails in certain cases

PR 7475687: Interpart Project with offset giving incorrect result



PR 7376599: Honor hidden explode flow line in drawing views with explode configurations

PR 7445736: undesirable segments remained after converting a view to 2d

PR 7454662: a custom property named "Positionsnummer" does not work anymore since ST6

PR 7460592: If there is not 3D model, the dimensions of the Dft file move

PR 7467096: Problem with dimension placement

PR 7476472: Dimensions disappear when they open the Dft file in "Inactive"

PR 7479182: When there is not 3D model/ open Inactive, Feature Control Frame becomes longer

PR 7481474: Parts List item numbers are N/A on file open when file is opened inactive

PR 7488330: Linear dimension moves if draft file opened without 3D data /Inactivate dwg view

PR 7494666: When there is not 3D model, the dimension moves

PR 8508749: Dimension moves far away when used attach dimension

PR 8510182: Linear dimension moves if draft file opened without 3D data /Inactivate dwg view

PR 7400253: Fixed sectioning failures for some models

PR 7495622: Parts List not displaying frame items


===Part/Profile/Sheet Metal===

PR 7448157: sheet metal part can no longer be edited

PR 7510126: Not possible to connect to multiple elements



PR 7450577: Sporadic error message when creating a copy of a dft file with Revision Manager


===Insight Connect===

PR 7481541: API Regression since ST 7 MP7 concerning Revman


===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7462078: Custom Properties can't be added to the BOM Report


===Solid Edge Embedded Client===

PR 1996834: Document Name formula problem within API, window will not update

PR 7429671: Initial value required attribute not available in ATT Interactive

PR 7428885: Create a new part returns a TC error



PR 7465071: Dxfout - Save As Flat: Etch Text alignment (Centered) exported as left justified



Fred White
Siemens PLM Software