Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 - Maintenance Pack 3 Announcement

Siemens Legend Siemens Legend
Siemens Legend

December 15, 2014

 

 

Dear Solid Edge Customer:

 

Solid Edge ST7 Maintenance Pack 3 for Solid Edge is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.

 

================

Download Location:

================

 

ST7 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST7/Maintenance_Packs/

 

==========

Installation:

==========

 

There were Solid Edge Embedded Client policy file updates in MP2. It’s vitally important that you install SEEC

Administrator, which delivers the policy files to TC_DATA.

 

Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 1127638: SheetSetup::GetDefaultDrawingViewScale method

PR 7231588: GetMappedPropertiesForGivenFile does not read properties from Part or Revision

 

===Assembly===

PR 7120417: unloading hidden parts leaving some subassemblies in a bad state

PR 7165893: Frame color changing when a 3D Sketch command is started

PR 7222695: dialog displaying when part is edited

PR 8250596: motor simulation regression

 

===Draft===

PR 1986693: Item count balloons that don't have a parts list are not updating

PR 2250765: Dimensions move when I open draft file in ST6

PR 7218956: Solid Edge crashes after using extend command

PR 7223291: Changing the fill style is not recognized when placing a section

               

===Part/Profile/Sheet Metal===

PR 7216664: Crashing when editing a protrusion in Simplify mode

PR 7226815: Save As translated -SE file extension is added to file name

PR 1128844: NX9 part can't be loaded and saved to ST6

PR 7223207: Tapered Thread input angle is ignored and defaults to 2.5° in Ordered

PR 7225894: Physical properties hidden after material is applied to model

PR 7189198: Simulation/deflection, color reflection on the part does not update correctly

PR 7232099: Cannot set material in Simulation Express.

PR 7240989 : Problem with BlueSurf with tangent end conditions creates dependency loop

 

===Insight===

PR 1992524: Too long time when saving a new draft file in Insight - Actions on asm and par

PR 1995321: Insight File open extremely slow - CPU intensive time during Deep Tree Generation

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 1996701: Part Title not mapped to Item Title

PR 7215405: Catch SP event mechanism failure needs to be back ported into ST7 MP

PR 8250103: Duplicate local check-out

 

===Solid Edge Embedded Client===

PR 1127691: ST6 removes TC-Absolute-Occurrence Information during upload/check-in

PR 1129564: SEEC Save As incorrectly displays Item Name in CPD when linked Item Rev exists

PR 7130564: SEEC Admin changes the values for item number synchronization when updated

PR 7182243: Replace one rev with another errors

PR 7183486: Save As of FOP member creates a SE Interpart Family link back to FOP master

PR 7225135: Revise creates wrong dataset name when specific custom property exists

PR 7182243: Replace one rev with another errors

PR 8252609: Save As with Structure Editor saves a wrong item name

 

 

Regards,
Fred White
Siemens PLM Software
1 REPLY 1

Re: Solid Edge ST7 - Maintenance Pack 3 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

SE4SharePoint server appears to be missing the file...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com