Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 - Maintenance Pack 6 Announcement

Siemens Legend Siemens Legend
Siemens Legend

April 7, 2015

 

 

Dear Solid Edge Customer:

 

Solid Edge ST7 Maintenance Pack 6 for Solid Edge is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.

 

================

Download Location:

================

 

ST7 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST7/Maintenance_Packs/

 

==========

Installation:

==========

 

There were Solid Edge Embedded Client policy file updates in MP2. It’s vitally important that you install SEEC

Administrator, which delivers the policy files to TC_DATA.

 

Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 7320225: Crash when using TextProfilesPtr GetCount on simple Sketch Text feature

PR 7325992: SetPropertiesInfo API does not allow the dataset name column to be cleared

 

===Assembly===

PR 7246804: Unable to access peer variables while in a sketch

PR 7250005: User was not able to edit frame

PR 7277410: Assembly crashes when opening

PR 7306907: Assembly aborts when opened

PR 7323166: Can’t create a second relationship with the assemble command

PR 8252662: Report in Assembly destroys User-Defined Mass of Sub-Assemblies

PR 7286889: Physical properties calculation saves material to part

PR 7295498: Parts jump on update all

PR 7319406: Assembly relationships fail after an assembly feature creation

PR 7336384: Solid Edge crashes when trying to place a T fitting

 

===Draft===

PR 7288091: DV become out of date, once an assembly has been opened

PR 7297427: Save as DXF regression from ST6

PR 7300422: Callout moves when open ST4 dft in ST7

PR 7304841: Repeated error message on mouse move

PR 7310012: Parts list update removes all rows for simplified sub-Asm

PR 7321142: same file name overwrite problem

PR 7322543: Draft file cannot be open and SE crash

PR 7251550: Automatic Coordinate Dimensioning very slow

PR 7324778: Drawing view of assembly doesn't default to no configuration

PR 8251882: Drawing View Properties / Style page shows the wrong style

PR 7315292: Slow Movement of Coordinate Dimensions

PR 7341723: Wrong dimension on broken revolved section view

 

===Part/Profile/Sheet Metal===

PR 1996595: Problem with shortcut key M in 3D IntelliSketch

PR 7203030: Cannot multi-select tangency handles while IPA'd into a part

PR 7321211: Combo box for sheet metal gage is too small in ST7 compared to ST6, regression.

PR 7308628: style if placed from Feature Library

PR 7335849: Crash while closing sketch with an active smart dimension/measure command

PR 7320068: Radial_Diameter_* is not properly adjusted if the Hole_*_Diameter is modified

PR 8250544: Insert sketch does not create a sketch

 

===Translators===

PR 7212861: Unable to open this SW file in Solid Edge.

PR 7303255: ST7 Crashes with SEPvTrn.ini file modified

PR 7306972: BOM View web part is crashing when selected

PR 7178850: Opening a SW assembly only translates the first part

PR 7254353: If unit is other than meter then JT generates model with white

PR 7296388: SolidWorks Data migration stops intermittingly

PR 7217433: Assembly constraints become corrupt when using MultiCAD driven references

 

===Insight Connect===

PR 7250363: Where used (search for asm) in revision manager very slow

PR 8253660: Rename of part and draft files breaks link from Drawing View to part file

PR 7206624: Labels missing for some commands when localized

PR 7334004: Cannot select Revision Rules when using UNC-defined Network Location

 

===Insight===

PR 8261109: Free Text Search and Where Use doesn't work

PR 7332037: Insert a new assembly by drag and drop “Cannot download a document”

PR 7307476: Impossible to add document number

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 1128335: SP Package File creation deletes Cache Content

PR 1970312: Pathfinder not displaying custom workflow status icons

PR 7226430: Support Multiple Site Collections Simultaneously in ST7 MP

PR 7239757: Files are not being uploaded to SESP

PR 8258870: Data Prep Tool Analyze reports File contains property without valid name

PR 1936459: SEEC Item numbers synchronization rolled back after AddToTeamcenter

PR 6958514: SESE revise is using the default NR and not the one used in the file

PR 7231415: SEEC & TC FCC error if working with weldment assemblies

PR 7294822: Revision Rules for Related Documents

PR 7159300: File Folders added to SE for SP are always lower case letters - hard to read 

PR 7288590: Performance problem when revising simple part and linked draft

PR 7332162: Drag and drop unmanaged part in assembly, incorrect symbol shown in path finder

PR 8259356: Workflow target is not valid for action Assign Status

PR 7312476: During upload of multiple MANAGED docs got errors that deleted the cache

PR 7312433: Search dialog takes 5-7 seconds just to display

 

===Solid Edge Embedded Client===

PR 7332854: does not assign project info, correctly during a revise operation

PR 7334006: Local BOM Precision Override

PR 8263114: AddToTeamcenter interactive doesn't honor the preference SEEC_property_item_name

 

Regards,
Fred White
Siemens PLM Software