Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 - Maintenance Pack 7 Announcement

Siemens Legend Siemens Legend
Siemens Legend

May 18, 2015

 

 

Dear Solid Edge Customer:

 

Solid Edge ST7 Maintenance Pack 7 for Solid Edge is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.

 

================

Download Location:

================

 

ST7 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST7/Maintenance_Packs/

 

==========

Installation:

==========

 

There were Solid Edge Embedded Client policy file updates in MP2. It’s vitally important that you install SEEC

Administrator, which delivers the policy files to TC_DATA.

 

Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 1128909: SegmentPointRelation3d.GetElement method fails on connection to other assembly

PR 7326618: API Interpart references are broken

 

===Assembly===

PR 1997310: thread feature fails in standard part screws

PR 7238389: Changes in Variable Table has no effect on other depending variable

PR 7288288: Handle points of frames moved after Update all links done

PR 7329238: Files opening with Read Only status when they are available

PR 7340152: Relation fails in assembly

PR 7340513: Crash when editing a multiple profile assembly feature

PR 7347154: not getting immediate feedback indicating that relationships have failed when IPA

PR 7351598: missing assembly features when opening from Draft

PR 7360551: Subassemblies being empty when any instances are not tagged "display in higher level"

PR 7339408: Cannot download the document message in open file dialog

PR 7345683: File units change for legacy files in ST7

PR 7286029: The values are overridden and updated in the SE options

PR 7343765: Missing properties on a Family of Assemblies - Please repair file

PR 8266361: System error encountered during evaluate while editing 3D sketch

PR 7283939: decimal places in assembly physical properties mass moment of inertia is locked

PR 7329334: Alternate Assembly previews not being correct

PR 7362568: not being able to edit a failed connect relationship

PR 7249140: Parts disappear from the display

 

===Draft===

PR 7328318: Property Text "Last printed date" will not be updated - wrong date on printout

PR 7234234: vertex edges were incorrectly suppressed in a section view of an assembly

PR 7235932: 3d connection device leaves fence select artifact

PR 7335228: Opening a DFT file crashes Solid Edge

PR 7337320: Block in Drawing View will not be exported

PR 7342543: Incorrect section view display

PR 7353124: Wrong dimensions in a Draft, when broken out section view exists

PR 8253818: Material Table > customer properties cannot be retrieved e.g. in Draft

PR 7304635: Shaded draft view colors inconsistent

PR 7360547: Repeatable ST7 crash in Draw In View

 

===Part/Profile/Sheet Metal===

PR 7339408: Cannot download the document message in open file dialog

PR 7345683: File units change for legacy files in ST7

PR 1996278: Unable to access edgebar features via API

PR 7295029: Deleting a hole profile locks Solid Edge if relationship colors are turned on

PR 7325679: Creating a 3D sketch, Solid Edge will crash

PR 7340095: SE crashes due to NULL pointer access

PR 7340385: Solid Edge crashes if a feature has the same name as the solid body

PR 7356608: Dimension Type Feature Callout slows down the graphics performance

PR 7357175: Hole feature changes geometry after editing the hole, that came via hole recognition

PR 7175521: Part dimensions change after doing a save-as

PR 7298290: Unable to repair web network

PR 7309165: Profile side changes direction when editing variables

 

===Translators===

PR 1991712: JT with long PMI causes crash

PR 7234372: Problems to import SAT files to ST7MP2, regression against ST6

PR 7294318: Document name Formula will not be taken in 3d PDF

PR 7351253: Solid Edge Viewer keeps psm files within an assembly opened for several minutes

PR 7355757: Save as jt not possible - Insufficient error message

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 1997720: Cannot sync exposed SE dimension variables to SESP numeric columns

PR 7172511: Pathfinder do not get update with the assigned numbers for drag n drop assembly

PR 7221411: BrokenLinkLog.xml does not include Alternates when running from cmd line

PR 7322191: Sync property values across part structure

PR 7340397: Where Used on sub-part, Revision.Title values not populated

PR 8265581: Content Browser shows only Favorite and Site Name - expand not available

PR 6974655: Numbering used to generate SE Standard Parts is incorrect

PR 7332477: Shen the browse folder is accessed from WC or EC there is bad performance

PR 7346513: Doesn't handle the Title (German Title) column as required

PR 7346893: Workflow Action "Update Drawings" creates unnecessary tasks

 

===Solid Edge Embedded Client===

PR 7283519: ASM occurrence property, Item Number are not being maintained from the TC BOM

PR 1993522: Revision field is blank in CPD when naming rule used

PR 7186212: Doing SaveAs of a NX driven reference assembly gives a Tc rules error

PR 7244837: Mandatory attribute in Teamcenter won't appear in "Add to Teamcenter" in SE

PR 7324478: SaveAs copies ItemRevision name from source to new object in 10.1.3

PR 7355261: Solid Edge Structure Editor not displaying the correct items

PR 7355760: Revise generates Partial Error

PR 7357577: create draft from model results in empty CPD

PR 7370456: Save as from managed draft does not properly do link fix up to new assembly

PR 7287253: Takes a very long time to open assembly files in SE Structure Editor

 

Regards,
Fred White
Siemens PLM Software
1 REPLY

Re: Solid Edge ST7 - Maintenance Pack 7 Announcement

Honored Contributor
Honored Contributor

Very good. About half of the sheet metal stuff applies directly to me and explains many crashes and slow downs I have experienced.