Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST7 - Maintenance Pack 9 Announcement

Siemens Legend Siemens Legend
Siemens Legend

September 4, 2015



Dear Solid Edge Customer:


Solid Edge ST7 Maintenance Pack 9 for Solid Edge is available for download.



The Solid Edge Team




Release Notes:



Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.



Download Location:



ST7 Maintenance Packs can be downloaded from:






There were Solid Edge Embedded Client policy file updates in MP2. It’s vitally important that you install SEEC

Administrator, which delivers the policy files to TC_DATA.


Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.


Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.



E-mail Notification:



To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.


To initiate your subscription, navigate to: for the web interface.



This Maintenance Pack addresses the following PRs:




PR 7418372: CommandInfo::Icon returns HICON of image list instead of a command icon bitmap

PR 7415571: API: ModelNode::GetCutLength returns 0

PR 7437107: The API 'ThreadDataByDescription' does not work in ST7

PR 7457728: constraint.GetGeometries API does not return the correct geometry



PR 7405944: not exiting the command when a subassembly becomes fully defined during placement

PR 7410611: Added Display Dimension control to the Occurrence API

PR 8264755: "Save Simplified Assembly As" failing

PR 1928569: Wrong Amount in "Atomic Parts List" (Reports and Draft)

PR 7413477: Expand All causing part files to load

PR 7423057: user is unable to copy sketch into opened Subassembly

PR 7432598: Updating all Open documents on each Peer Variable Table record update

PR 7439634: Item number blank and read only in occurrence properties in FOA files

PR 7446113: part status not correct when adding tangential relations

PR 7457275: Interference checking on construction surfaces in ST7

PR 7459332: not being able to drag a component in some scenarios when going between a selected edge and a triad axis

PR 7462671: inactive simplified subassemblies not being included in physical properties calculations.

PR 8506060: Break links does not exist on the edit links dialog in ST7

PR 7463722: "Display in Higher Level" setting will not affect physical properties calculations

PR 7470955: PMI Section view does not cut a fillet weld



PR 7384379: Unusual semi-circles appear in some dual dimensions

PR 7415256: Grid disappears when switching sheets

PR 7415586: Parts List changed unacceptable after update views

PR 7363506: Loop test does not include spreadsheet

PR 7376599: Honor hidden explode flow line in drawing views with explode configurations

PR 7405632: Tolerance becomes abnormal when I change a text scale

PR 7407307: Blocks on background sheets not exported to DXF

PR 7432084: Solid Edge crashed while reading entities

PR 7436337: Tangent command is in a bad state after pressing SHIFT and middle mouse button

PR 7440042: Drawing View Properties / Style page shows the wrong style

PR 8505679: Direction of displacement is reversed in the saved image


===Part/Profile/Sheet Metal===

PR 7421230: Crash when inserting feature library

PR 7392093: Driving dimensions do not accept decimal values

PR 7434569: KeyShot import issue

PR 7247507: Problem of changing geometry in Sheet Metal Assembly

PR 7271837: Deselected region reselected when green checkmark clicked

PR 7437087: Smart Dimension locks 2 files up - Please repair in ST7

PR 7441752: Transfer from styles via material.mtl doesn't work correctly

PR 7444567: Unusual semi-circles appear in some dual dimensions

PR 7448157: Sheet metal part can no longer be edited



PR 7398888: Difference in assembly contents and relationship when opened with different user

PR 2215861: SaveCopyAs changes Author value in Summary Property to Windows User Name

PR 7143583: Revise via SE is changing the author property

PR 7361387: Unit Tolerance for Insight Managed files doesn't work - Dot / Comma problem


===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7387776: Crash seen on sending part to RB which saved under a folder that has "," in name

PR 7408925: SESP Client performance slow on Address -> Select Folder dialogue

PR 7431109: Select Folder dialog for New Document is incomplete if Windows Display is 150%

PR 8274706: SESP workflow issues: SESP people picker web part takes lot of time to load


===Solid Edge Embedded Client===

PR 6971928: Save As- PDF for draft does not exist under new item revision

PR 7412957: Multiple scenarios where SESE will either crash or freeze

PR 7429671: SEEC: Initial value required attribute not available in ATT Interactive

PR 7458795: SEEC - revise all of a complex structure assembly does not finish

PR 8263114: AddToTeamcenter interactive doesn't honor the preference SEEC_property_item_name



PR 7426671: Solid Works files won't open in Solid Edge

PR 7428388: On some parts of the assembly SE in sync mode cannot recognize holes

PR 7428887: Export to 3D pdf, KeyShot, SEV creates several instances of the same part copy

Fred White
Siemens PLM Software