Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Solid Edge ST7 is sluggish

Builder
Builder

Is it just me or is Solid Edge becoming so blotted that it needs to be constantly hand held for it to work normally OOTB...........Been around SE now for years and countless versions and not really sure it heading in the right direction??  

 

Hope not though?

ST9
WIN 7Pro 64bit
DELL T5810 3.7-4Ghz 32Gb ECC

Re: Solid Edge ST7 is sluggish

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not seeing that here as long as graphics drivers are kept up to date.  Seems Win 10 is still going through growing pains and every large update impacts graphics drivers requiring the vendors to react and produce a new driver.  Luckily we run the Enterprise edition of Windows which delays Windows Update for a few months till the updates are road worthy versus the other editions that get them right away.  I know the Fall Creators Update that was just released introduced an issue in SE with Quadro cards that the latest driver may fix...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com