Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 - Maintenance Pack 10 Announcement

Siemens Legend Siemens Legend
Siemens Legend

August 23, 2016

 

Dear Solid Edge Customer:

  

Solid Edge ST8 Microsoft Installer (MSI) Maintenance Pack 10 is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Beginning with Solid Edge ST8, Maintenance Packs are delivered as and installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are installed and tracked as Product Updates.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling a MSI Product Update will restore the installation to the state before the Product Update was applied.

 

  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation. After the current Update is uninstalled, the previous Update will become the current Update, if there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).

 

Solid Edge Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to 15 months following the release date of the English version. The release date for Solid Edge ST8 English was 06/05/15, making the Maintenance Pack cutoff date 09/05/16.

 

Solid Edge - Solid Edge ST8 supports Windows 10 if the Windows 10 “November Refresh” version 1511 (OS Build 10586.0) or later is installed.  Solid Edge does not support the new Windows 10 browser, Microsoft Edge.

 

Solid Edge Integration to Teamcenter - The Solid Edge integration to Teamcenter 10.1.5 and later have been tested on Windows 10 connected to Teamcenter 10.1 and 11.2 servers and there are no known issues.  Teamcenter plans to announce support of Windows 10 with Teamcenter 10.1.6 and 11.2.2.

 

================

Download Location:

================

 

ST8 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST8/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack Executables (.exe files) deliver updated versions of existing product dlls.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be uninstalled using Uninstall a program from the Control Panel.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Assembly===

PR 7588050: After unloading hidden parts from memory, show parts crahes Solid Edge

PR 7744701: Pattern along curve wrong in ST8MP8, ok in ST7 and ST9, regression

PR 8709792: Opening Draft file over the network is slower

PR 7629696: Project to sketch fails when IPA

PR 7720634: Conflicting relationship message because of a mirror object not being up-to-date

PR 7726186: Not able to remove mass in variable table.

PR 7775478: Assembly is unable to close after deleting a sketch

                                                                                                                                                          

===Draft===

PR 7742348: Angular dimension makes Solid Edge close after editing

PR 7750164: Coordinate dimensions alignment dashed lines won’t go away

PR 7749657: Crash during open of an Symbol = Title Block on the background sheet

PR 7754000: Distance Dimension by two points displays at wrong location after using zoom

PR 7763216: Wire harness elements becoming disconnected

PR 7769914: Overwriting of sheet numbers in a title Block, when saving as PDF.

PR 7706846: Lock-up while entering Property Text in a text box rec

 

===Part/Profile/Sheet Metal===

PR 7727602: Pulldown-Menu to small, names not visible

PR 7731394: Material Names with a "." in name changes to "," only in German version.

PR 7736718: Argument Exception with Threads.Add - Example required

PR 7746098: Command fails when all features in Sync but you run cmd in ordered env.

PR 7491674: Japanese text is not shown while inputting Japanese text in Command finder field

PR 7764181: The preview window obscures the search results

 

===Insight Connect===

 

===Insight===

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7562274: Standard Part Name will not be written to SESP Revision.Title

 

===Solid Edge Embedded Client===

PR 7726588: FOA Save/check-in failure

PR 7734168: Structure Editor not building new assembly correctly when using SmartCodes

PR 7741423: Problem with revision rules after revision subassemblies SE-TC

PR 7756122: Structure Editor "Save as" doesn't relink some views

PR 7741423: Problem with revision rules after revision subassemblies SE-TC

 

===Translators===

PR 8307275: API, SaveAsJt Use_Simplified_Part argument sill not working in MP8

PR 7749517: Solid Works-Data can't be imported

Regards,
Fred White
Siemens PLM Software