Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 - Maintenance Pack 9 Announcement

Siemens Legend Siemens Legend
Siemens Legend

 Jun 13, 2016

 

Dear Solid Edge Customer:

  

Solid Edge ST8 Microsoft Installer (MSI) Maintenance Pack 9 is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Beginning with Solid Edge ST8, Maintenance Packs are delivered as and installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are installed and tracked as Product Updates.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling a MSI Product Update will restore the installation to the state before the Product Update was applied.

 

  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation. After the current Update is uninstalled, the previous Update will become the current Update, if there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).

 

Solid Edge Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to 15 months following the release date of the English version. The release date for Solid Edge ST8 English was 06/05/15, making the Maintenance Pack cutoff date 09/05/16.

 

Solid Edge - Solid Edge ST8 supports Windows 10 if the Windows 10 “November Refresh” version 1511 (OS Build 10586.0) or later is installed.  Solid Edge does not support the new Windows 10 browser, Microsoft Edge.

 

Solid Edge Integration to Teamcenter - The Solid Edge integration to Teamcenter 10.1.5 and later have been tested on Windows 10 connected to Teamcenter 10.1 and 11.2 servers and there are no known issues.  Teamcenter plans to announce support of Windows 10 with Teamcenter 10.1.6 and 11.2.2.

 

================

Download Location:

================

 

ST8 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST8/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack Executables (.exe files) deliver updated versions of existing product dlls.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be uninstalled using Uninstall a program from the Control Panel.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Assembly===

PR 7546456: Editing a revolved cut-out does not cut new part

PR 7719850: Frames do not display on IAC or mirror components

PR 7585893: Assembly Feature Compute is slow

PR 7735777: Lost quality saving as image (JPG) from ST6 to ST8

PR 7738036: KeyShot and 3dpdf export is incorrect with assembly features

                                                                                                                                                          

===Draft===

PR 7719757: Stack pitch varies on save and reopen

PR 7725738: A view that used a configuration with simplify states did not update to show the correct state

PR 7731631: Feature Library sweep is way off of cross section curve with Plane normal to curve

PR 8300567: Block origins and its dimensions are not at the correct position

PR 7738107: Crashing when placing blocks.

 

===Part/Profile/Sheet Metal===

PR 8703479: pattern from hole in a psm file takes too long to process

PR 7620508: Material of the FOP elements is not definable via the property manager

 

===Insight===

PR 7723901: Missing parts in ASM PathFinder and on display after change to Designed ASM

PR 7649873: IPA a subassembly then select upload all vs Upload

 

===Solid Edge Embedded Client===

PR 7731270: Yes/No Column values not added to BOM Report if created via Workflow

PR 7669623: ATTI can't import part and draft together on a MultiSite environment

PR 7723217: SEEC gives error if GRM forbids more than one SE Draft per ItemRevision

PR 7728083: Save As All of structure with non CAD and CAD parts does not work as expected

PR 7734002: Structure Editor save as from draft creates wrong part file name

PR 7742005: BOM Sync is not working properly after Toggle Precise/Imprecise in Tc

PR 7684695: Missing files when opening an assembly from Teamcenter

PR 7717871: AtTI closes with error when trying to create a new session

PR 7710652: The Rev naming rule is not reflected in the dataset name

PR 7722996: Open DFT with links other DFT files are not downloaded to cache folder

PR 7729554: Performance - Open Assembly

PR 7667301: Template cannot be found for deleted Asm opened from MRU

PR 7736397: Save Alternate Assembly does not upload Arrangement to Teamcenter

 

===Translators===

PR 7731045: Solid EdgeTranslationServices.exe does not translate a psm to igs/stp anymore

 

Regards,
Fred White
Siemens PLM Software
2 REPLIES

Re: Solid Edge ST8 - Maintenance Pack 9 Announcement

Phenom
Phenom

Is this due to MP9?

2016-07-14 11_32_56-Solid Edge ST8 - Ordered Part - [Part2].png

...........................................................................................................
Solid Edge ST10 & AutoCAD 2019 user

Re: Solid Edge ST8 - Maintenance Pack 9 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

On my MP9 the Revolve tooltip is working as expected -- in both Ordered and Sync.