Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 - Standard parts problems

Master
Master

Hello all,

I have installed ST8 and want to re-use the StdParts.

 

I have used a Dutch version for installing the StdParts, the file location is on the server.

After 30 error windows with a preview2 folder problem it is installed.

However, now I cannot start the StdParts Administrator from my start menu.

 

Is there a different work method or something? Is it that hard to make a good working version of Standard Parts? For a keyuser it starts to get at the level of a IT-employeeSmiley Frustrated

 

See the attachment for the file that I have used, page 22.

3 REPLIES 3

Re: Solid Edge ST8 - Standard parts problems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That document is for ST3.  I suggest you get the one for ST8 as I believe some things have changed since then and it will probably also have information on how to upgrade from a previous versions database.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST8 - Standard parts problems

It should not matter right?
But with support from our dealer it works great.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Solid Edge ST8 - Standard parts problems

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi,

 

Is it a SQL error? If SQL have error try install latest sql express from web. It's free.

 

Also can try this method:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Solid-Edge-ST8-Standard-Parts-SQL-S...