Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 System Requirements and Information

Experimenter
Experimenter

I have a MSI, and it has the screen in resolution 4K, the icons in the program are too smalls, because I think that the resolution of the screen is too big than the program. I try to change the resolution of my screen, only HD, but it does not work well. The text of the program, it looks great, but the icons no. I need help.

 

If you can answer in spanish. Thank you very much

 

5 REPLIES

Re: Solid Edge ST8 System Requirements and Information

Siemens Phenom Siemens Phenom
Siemens Phenom

ST9 was the first version to provide support for high-res monitors.  Please see page 18 of the ST9 What's New document:

 

https://support.industrysoftware.automation.siemens.com/docs/se/st9/sev9releasenotes.pdf

 

Re: Solid Edge ST8 System Requirements and Information

Gears Phenom Gears Phenom
Gears Phenom

try the option to make the icons larger.

5-9-2017 8-21-55 AM.png


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Solid Edge ST8 System Requirements and Information

Experimenter
Experimenter
Where?

Re: Solid Edge ST8 System Requirements and Information

Gears Phenom Gears Phenom
Gears Phenom

SE Options - from the Application Button.   Top Left most SE Icon...

 

Im in ST9 and my UI is a bit diffent so i can not screen shot it...


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Solid Edge ST8 System Requirements and Information

Valued Contributor
Valued Contributor

ST8

 

2017-05-09 15_55_46-Solid Edge Options.jpg


CAD/CAE Manager
ST8 MP12