Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 Viewer does not allow me to open second file

Genius
Genius

Hi,

 

I'm testing the free Solid Edge ST8 Viewer at home. If I try to open a second file from the File/Open dialog, I get an error message. If I rightclick a SE file in Windows Explorer and choose Open with > Solid Edge Viewer it works fine (blue mark).

 

I've never seen this problem in ST7 or earlier versions. 

 

Can somebody replicate this? Is this a new restriction and regarded Works as Designed?

 

Cannot_open.JPG

 

Regards,

Robin.

2 REPLIES

Re: Solid Edge ST8 Viewer does not allow me to open second file

Community Manager Community Manager
Community Manager

There is a the new ‘Add’ button to open multiple docs in the same PCF.

See attached jpg.

 

Laura

 

Re: Solid Edge ST8 Viewer does not allow me to open second file

Genius
Genius

OK thanks, works fine. A little counterintuitive though.