Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 non resposive

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

 

I am System admin , We have 12 designer , We have just upgrade Solid Edge from ST7 to ST8. We access the data over the centeral server which is in LAN. Speed is quite good for lan . I can get ping in 1 ms to server. Our workstation Hardware is 12 to 16 GB RAM 4 GB Graphics card 1 T
B space. Prroblem is after upgrading now 12 of my users complining that solid edge is hangs while saving or by any other changes. He has to close the task through task manager only. I have check the rest of the hardware use . CPU uses are quite normal 3% , RAM 8 % Network nill. REst of the software work fast and correct. Please any one send me the solution urgently.

 

Tushar Joshi

 

it.support@grindmaster.co.in

8983571007

2 REPLIES

Re: Solid Edge ST8 non resposive

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

The first suspect in such cases is always the virus scanner.

 

To test this you have to uninstall the scanner on one PC to see if there are differences.

Just deactivating of the scanner will sometimes not really deactivating the scanner function. Be on the safe side and deinstall the solution.

 

Stefan

 

 

 

smitsch@unitec.de
www.all4edge.de
Highlighted

Re: Solid Edge ST8 non resposive

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Further to that which @Stefan_Mitsch says....if you haven't already, I recommend you download & install the latest maintenance pack [MP3], in case there are advancements included there, that could help with your issue.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019