Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 on Tablett Dell Venue Pro 7140

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

We try to work with Solid Edge on a Dell Tablett PC

 

Dell Venue 11 Pro 7140

 

But Solid Edge is crashing whenever we try to create a new 3D-Featuer like Extrusion.

You can open existing 3D-Modell (Parts &Assemblies). This works fine but when you try to add a feature Solid Edge crashed.

 

Even the Option Graphiksupport  "Software" will result in a crash.

 

Any  suggestions out there?

 

Thank You

 

Stefan

smitsch@unitec.de
www.all4edge.de
4 REPLIES

Re: Solid Edge ST8 on Tablett Dell Venue Pro 7140

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Stefan_Mitsch,

 

I have nothing to offer as a solution sorry, but only to say, I guess this reinforces the unfortunate reality that not all PC's, tablets included, are created equal, even with comparable hardware.

There might be some [wild guess here Robot wink ] emulator somewhere, that is just not tuned right for Solid Edge to work correctly.

 

I am, even today, amazed by the performance on a Surface Pro3, and seeing them at SEU15, the newer Surface Pro4 & Surface Book devices are even more so.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Solid Edge ST8 on Tablett Dell Venue Pro 7140

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Stefan,

I think that your issue looks very much like a graphics issue. According to my local Dell website the Dell Venue uses the Intel® Core™ M-5Y71 cpu and this has the Intel® HD Graphics 5300 which "should" work OK.

I would make sure that you make sure that you have the latest graphics driver from Intel.

Cheers

Mark

Re: Solid Edge ST8 on Tablett Dell Venue Pro 7140

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

We updated the driver for the Videocard but still face the problem with the crashes.

 

It seems to me that this HW is not suitable for Solid Edge. Are there other experiences out there with a Tablet PC?

Surface Pro from Microsoft is known.

 

Thank you

 

Stefan

 

smitsch@unitec.de
www.all4edge.de

Re: Solid Edge ST8 on Tablett Dell Venue Pro 7140

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Does it have a supported operating system?
LMGi
www.TLMGi.com