Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 requirement and compatible with Win 10?

Experimenter
Experimenter

Hi, may i know Solid Edge ST8 is compatible with Windows 10 pro 64-bit? Is there any requirement for graphic card? I plan to buy Acer laptop travelmate P249-M-55TD if windows 10 not supported, just wonder Intel HD graphics 520 on this laptop is sufficient for ST8 or not. Thanks for reply.

3 REPLIES 3

Betreff: Solid Edge ST8 requirement and compatible with Win 10?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @fg4q7775

 

 

 

Win10 has done a good job with ST8 as well as with ST9 and ST10.

 

And the Intel Onboard graphics also have shown real good behaviour with Solid Edge,
even with assemblies of 2000 parts/subassemblies.

 

I can not say if - or I suppose it will not be - the best choice for bigger assemblies.

 

In general I was surpirsed how SE is running on "standard" tablets like the Surface Pro and similar.

 

 

regards
Wolfgang

Betreff: Solid Edge ST8 requirement and compatible with Win 10?

Legend
Legend

Hello @fg4q7775,

It is possible to use ST8 MP3 or newer with Windows 10.

HD on board CPU graphic can be good too.

However, for SE model that need more power from a GPU an additional GPU can be a good solution.

Workspace use is here also to calculate.

How much parts/asm you like to use with SE at this laptop?

Will you create 2D drawings?

How many external files you like to convert with the laptop?

 

Solid Edge System Requirements and Information

 

Best Regards

Wolfgang

 

 

Betreff: Solid Edge ST8 requirement and compatible with Win 10?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

My personal laptop is a an Asus I5 2.2ghz, 8gb ram, HD 5500 graphics on Win10 Home (64 bit) and it runs SE pretty well. I don't use it often but I wouldn't hesitate for modest assemblies keeping in mind @Wolfgang_1's caveats.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200