Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST8 with Keyshot 7

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello!

 

I had installed Keyshot 7 in a computer with Solid Edge ST7. There is a problem now using Keyshot and View and Mark.

 

When is needed to use both programs the next error appears:

"C:\Program Files\Solid Edge ST8\ Program\wim32\DOCMGT.DLL is not designed to wun on Windows or contains an error. Try to install the program again through the original installation media , or contact the system administrator, or the sofware manufacturer for help Status of error 0xc0000020"

(directly translate from Spanish)

 

To solve it I made the following steps:

1. open the cmd as administrator

2. write "cd C:\Program Files\Solid Edge ST8\Program\win32" and press "enter"

3.write "regsvr DOCMGMT.dll" and press "enter"

4. now a message appears saying that the dll was registered propertly.

 

It works for some time, but now happens again.

 

¿You may know any other solution?

9 REPLIES

Betreff: Solid Edge ST8 with Keyshot 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @BeatrizSeoane

 

 

Yes, IMHO the best way always would be to keep it eas it is intend to be!

So with ST7 I would use the Keyshot version which comes with SE and nothing more.

 

I have seen last week, that KeyShot 7 works with ST8 with minoproblems only, but those keep the same to ST10 too.

 

regards
Wolfgang

Betreff: Solid Edge ST8 with Keyshot 7

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
So, It may be one of that microproblems?

Betreff: Solid Edge ST8 with Keyshot 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @BeatrizSeoane

 

 

 

no this sounds to be bigger.

 

 

regards
Wolfgang

Betreff: Solid Edge ST8 with Keyshot 7

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
hahahah
And any idea to solve it?

Betreff: Solid Edge ST8 with Keyshot 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @BeatrizSeoane

 

 

 

I would try to uninstall Keyshot7 and reinstall it from Solid Edge DVD version ST7

 

 

regards
Wolfgang

Betreff: Solid Edge ST8 with Keyshot 7

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I need to work with Keyshot 7, do you recommed me to install it again after the reinstallation?

 

Thank you!

Betreff: Solid Edge ST8 with Keyshot 7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @BeatrizSeoane

 

 

 

this IMHO is not matter of recomendation or not, 
if You say "You need to work with KS7", then there is no other way, isn't it?

 

I have seen that with ST8 Keyshot7 was being able to be used.

You first have to uninstall KS6 and to install KS7 afterwards

 

So far it worked fine.

 

 

regards
Wolfgang

Betreff: Solid Edge ST8 with Keyshot 7

Siemens Phenom Siemens Phenom
Siemens Phenom

Betreff: Solid Edge ST8 with Keyshot 7

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello @uk_dave and @hawcad,

 

now I uninstall Keyshot 7 and repair solid Edge. I still having the same problem.

 

Any idea?

 

Thank you