Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 Certified

Creator
Creator

Good Afternoon Srs,

 

How I visualized who you are well experienced in SolidEdge certifications.

I am from Brazil and am having divergence in my solidEdge certification, If it does not disturb you, could you help me? It refers to the value imputed in the response box.

 

Calculation of volume:

Result shown on solidedge:

 

1.png

 

I put the value in the answer box: 1620426945. 

 

2.png

 

Distance:

Result shown on solidedge:

 

3.png

 

I put the value in the answer box: 18096. 

 

4.png

SolidEdge says that it's wrong

 

I was disapproved twice for this divergence, could you tell me what would be the correct value as the example above?

 

Att,

 

Wendel Trento

4 REPLIES

Re: Solid Edge ST9 Certified

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@WendelTrento,

 

Already replied to this in your last post........but again, it looks to me, that you have omitted the decimal points in both of your answers. Include or remove them, and see if that helps you.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge ST9 Certified

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello Wendel,

 

In your answers to the certification test questions, you should use integers - whole numbers with no decimal fraction - in your answers.  So the first answer would be 1620427, and the second answer would be 181.

 

Best regards,

Kevin Riggs

Manager, Solid Edge Learning Media Development

Re: Solid Edge ST9 Certified

Legend
Legend

I think the confusion might come from how thousand seperators & decimal fractions are seperated in different countries.

 

In most english speaking countries one thousand = 1,000.00

In many non-english speaking countries on thousand = 1.000,00

 

Could see how this could cause confusion, there may be an option in settings to format numbers as you are used to them.

Solid Edge 2019 MP4 - Windows 10 - K2000

Re: Solid Edge ST9 Certified

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

You're right, Dave, this is the problem.  At this time, the system does not handle decimal separators internationally, and it is not possible to resolve this with settings.  This is why answers should be whole numbers, rounded to the nearest integer.