Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Common Views Command is Missing in Ribbon Bar - View

Creator
Creator

We are using Common Views command regularly to adjust/fix the view of part/assembly at required position.

In ST9 we couldn’t find this command icon on the view Ribbon bar.

But this command is available in ST9, we can add this in Quick access bar, Radial Menu and can create a key board shortcut but cannot add it on Ribbon bar.

Below step will use to add the common views on Quick Access bar.

 

  1. Right Click on Ribbon bar, Select Customize the Ribbon…
  2. Select the Environment such as Assembly/Part/Sheet metal (need to perform separately).
  3. All Commands… select Common Views
  4. Close the Dialogue Box, then Save the changes on the theme.

 

3 REPLIES 3
Highlighted

Betreff: Solid Edge ST9 - Common Views Command is Missing in Ribbon Bar - View

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

and what#s about the "Viewing Cube" which was implemented with ST8?

 

This IMHO has taken over the functionality of the former "Common View"

Nevertheless the Common View is available, e.g. in the lower right area of viewing commands

Here You can put it and always will find it.

 

To You see any davance by the CommonView against the Viewing Cube?

 

 

regards
Wolfgang

Betreff: Solid Edge ST9 - Common Views Command is Missing in Ribbon Bar - View

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @DNSKMR,

 

I was just going to mention the same as Wolfgang......also, you could activate [check box] the "Common Views" function from "Status Bar" set, by right clicking on the any of the existing group.

 

I think the "Quick View Cube" is better, and easier by far, than common views.

 

ST9_StatusBar_CommonViews.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Solid Edge ST9 - Common Views Command is Missing in Ribbon Bar - View

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SeanCresswell

 

 

thanks for picture and the English name of the "Status Bar"

 

Since I'm using a German Version of SE I was not familiary with the original name of it.

 

 

regards
Wolfgang