Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - File Properties - Part and Sheet Metal Environment

Experimenter
Experimenter

I used to enter Custom File properties such as material, Description etc in part and Sheet metal environment.. And these attributes will picked into customer made part list in Draft file. This is usual practice and worked out effectively with previous versions.

But In ST9 File properties, I faced an issue with Material Attributes. Material is already available in standard as Physical; if I try to add in Custom hits an error like Material is already available. I could not delete the existing Material Properties under Physical column. I need to enter the material value which has different naming (not standard/commercial material) Can anyone help to solve the issue?

2 REPLIES

Betreff: Solid Edge ST9 - File Properties - Part and Sheet Metal Environment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



I just was able to add an user defined property with name "material".

 

Using ST9 MP1

 

 



regards
Wolfgang

Re: Solid Edge ST9 - File Properties - Part and Sheet Metal Environment

Honored Contributor
Honored Contributor

With sheet metal, an extra step/connection can be involved. The Gage. The material could be associated with the gage, and the gage selection is in control. Or not. Depends if you associate materials with gages.