Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 10 Announcement

Siemens Legend Siemens Legend
Siemens Legend

September 14, 2017

 

Dear Solid Edge Customer:

  

Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 10 is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.

 

=============

Update Version:

=============

 

109.00.10.04

 

================

Download Location:

================

 

ST9 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling an MSI Product Update will restore the installation to the state before the Product

  Update was applied.

 

  • PLEASE NOTE: When uninstalling an MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail

notification.

 

For details on initiating your email subscription navigate to:

http://support.industrysoftware.automation.siemens.com/general/email.shtml

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Part/Profile/Sheet Metal===

PR 8927848: Editing synchronous slot aborts the product

PR 8950444: Product crashing often when working with the variable table

PR 8934329: Unacceptable delays when opening part files with Excel links

PR 8943325: Unable to copy color while doing part copy

PR 8951650: Random abort when working with the draft copy command

PR 8345587: Solid Edge aborts when double click on user variable value in VT

PR 8957335: Material in Pathfinder out-of-date

 

===Assembly===

PR 7478257: User can select a FOA member on File -> Open while another member is active

PR 8919002: an abort in Assembly

PR 8948791: abort on selecting edge from a bad slot feature to place asm relation

PR 8346579: CustomOccurrenceProperty.xml Properties with Invalid behavior types added to asm

PR 8920113: SE-User defined mass not carried into upper level assembly

                                                                                                                                                          

===Draft===

PR 8513742: Japanese vertical text is not displayed correctly in Windows

PR 8858589: Callout with value of surface area does not update when surface area changes

PR 8867357: Caption of 2D view moves, when opening ST4 Draft in ST9

PR 8867258: Break line extends when opening in ST9

PR 8887266: The draft File with 3D File and without 3D File are different

PR 8535286: Dimension disappears when active window changes

PR 8944461: Solid Edge terminates Windows with Bluescreen - Zoom Draft View with tif image

PR 8928941: Fixed a sectioning error due to Boolean failure

PR 8943239:  If we changed a size of BMP on draft, ST9 changes size downward

PR 8958874: Aligned view incorrect when principle view is oriented with Look at face

PR 8959448: Problem re-attaching symmetric dimensions

 

===Translators===

PR 8957904: Line missing in dxf when using save as flatten

 

===API===

PR 8954367: Exception on close in visual.dll when using SEPreview.ocx

PR 8949119: Tube.Path(objNPaths) throws an exception in ST9

PR 7993126: ST9 custom addin menu is devided two tabs using API of AddCommand.

 

===General===

PR 8333251: user-specific paths cause saving problems after deploying sepref to another user

PR 7925571: Performance for Open new Part/PSM/ASM is SLOW

PR 8901488: New revisions for all FOP members are not replaced in assembly in below workflow

 

===Insight===

PR 8900552: Asm cfg can't be saved and other strange behavior after use of Save As Copy

 

===Teamcenter Integration for Solid Edge===

PR 7767962: The last_released_status property does not map correctly in SEEC

PR 8957604: SEEC: Item Number column in Occurrence Properties disappears

PR 8919610: SETranslationsServices generates application error while converting dft to pdf

PR 8934757: AtT: Stops functioning when selecting different group roles via cache

PR 8945903: SEEC crashes when opening FOA from MRU after new member created

PR 8945903: SEEC crashes when opening FOA from MRU after new member created

PR 8917637: SEEC: Project Name displays Item Name instead of actual value for Project Name

 

===Built-in Data Management===

PR 8937432: Unregister SEPropertyhandler.dll, windows event log does not capture the process

 

===Design Manager===

PR 8902403: Design Manager: Unexpected overwrite message is shown during Save As

PR 8947721: Where Used process crashes with a Close Program error when selecting Recursive

PR 8886062: Design Manager with Insight don't maintain the column setting

PR 8901842: ST8 aborts using Property Manager

 

===Mold Tooling===

PR 8894127: Associative with Material is unchecked at Material Dialog reopen.

 

Regards,
Fred White
Siemens PLM Software
8 REPLIES 8
Highlighted

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Readme file says:

 

Microsoft Installer (MSI) Maintenance Pack

Product: ST9 MP9
Version: 109.00.10.04

 

I guess it is a copy paste forget

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Valued Contributor
Valued Contributor

Fast Search is still not working after MP10 installation. Do I need to re-register the dll manually?

 

I installed the MP as administrator but I'm using SE as regular user, may be this could be the reason for the forgotten registration of the DLL? I don't know if this DLL work in user-space or for all-users.

____________________________
http://www.stimarchetti.it
Design of automation

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Gears Phenom Gears Phenom
Gears Phenom

@Alessandro wrote:

Fast Search is still not working after MP10 installation. Do I need to re-register the dll manually?

 

I installed the MP as administrator but I'm using SE as regular user, may be this could be the reason for the forgotten registration of the DLL? I don't know if this DLL work in user-space or for all-users.


Fast search were fixed with MP9 but with a separate update file (Fast_Search_MSI_MP9.exe)

 

Do you mean with MP10 it's broken again ?

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Valued Contributor
Valued Contributor

After MP 10 installation the fast search feature does not work, but I didn't tested if it worked before installation. I'm sure it worked a few day ago with MP9 installed, but a big Windows update happened in the meanwhile.

 

At least the MP10 installation didn't fix the problem, but it is also possible that it broke something that worked before MP10 installation. It is also possible that the responsable is the last windows update too.

 

I registerd the DLL as regular user but with no success. After that, I did it as Administrator and now Fast Search works again, I guess until the next rain in the other side of the world... Smiley Very Happy

 

____________________________
http://www.stimarchetti.it
Design of automation

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@Alessandro we have just been made aware of a particular issue with MP10 Fast Search on Windows 10.  This issue is not widespread and does not reproduce on all Windows 10 systems.  We are actively investigating this issue now.

 

Please contact your Solid Edge support person and submit an IR to GTAC.  In your IR please reference existing PR 8978423.


Again, this is not occurring for all systems and at this time appears to be limited to only a few select systems.

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@Alessandro P.S. When you get your IR submitted to GTAC please PM me the IR number and I will actively pursue getting this moved forward for you.

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave, can you share the symptoms of this issue?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST9 - Maintenance Pack 10 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@KennyG for the particular issue reported in PR 8978423, after installing MP10, the out-of-the-box Solid Edge properties are then missing from indexing but any custom properties are still being indexed.  Re-registering the dlls [as with most indexing issues] should resolve the issue.