09-14-2017 01:59 PM
September 14, 2017
Dear Solid Edge Customer:
Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 10 is available for download.
Sincerely,
The Solid Edge Team
============
Release Notes:
============
Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and
installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked
as Installed Updates.
=============
Update Version:
=============
109.00.10.04
================
Download Location:
================
ST9 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/
==========
Installation:
==========
Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be
uninstalled using Uninstall a program from the Control Panel.
with a lesser version.
in MP1 and MP2.
been cases where the Disk Space Computation takes several minutes to complete. Please be patient.
Update was applied.
Product Update package, if any, must be available to allow the recovery of previous file versions.
After the current Update is uninstalled, the previous Update will become the current Update, if
there were multiple Updates installed.
updates -> Uninstall).
===============
E-mail Notification:
===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail
notification.
For details on initiating your email subscription navigate to:
http://support.industrysoftware.automation.siemens.com/general/email.shtml
=========================================
This Maintenance Pack addresses the following PRs:
=========================================
===Part/Profile/Sheet Metal===
PR 8927848: Editing synchronous slot aborts the product
PR 8950444: Product crashing often when working with the variable table
PR 8934329: Unacceptable delays when opening part files with Excel links
PR 8943325: Unable to copy color while doing part copy
PR 8951650: Random abort when working with the draft copy command
PR 8345587: Solid Edge aborts when double click on user variable value in VT
PR 8957335: Material in Pathfinder out-of-date
===Assembly===
PR 7478257: User can select a FOA member on File -> Open while another member is active
PR 8919002: an abort in Assembly
PR 8948791: abort on selecting edge from a bad slot feature to place asm relation
PR 8346579: CustomOccurrenceProperty.xml Properties with Invalid behavior types added to asm
PR 8920113: SE-User defined mass not carried into upper level assembly
===Draft===
PR 8513742: Japanese vertical text is not displayed correctly in Windows
PR 8858589: Callout with value of surface area does not update when surface area changes
PR 8867357: Caption of 2D view moves, when opening ST4 Draft in ST9
PR 8867258: Break line extends when opening in ST9
PR 8887266: The draft File with 3D File and without 3D File are different
PR 8535286: Dimension disappears when active window changes
PR 8944461: Solid Edge terminates Windows with Bluescreen - Zoom Draft View with tif image
PR 8928941: Fixed a sectioning error due to Boolean failure
PR 8943239: If we changed a size of BMP on draft, ST9 changes size downward
PR 8958874: Aligned view incorrect when principle view is oriented with Look at face
PR 8959448: Problem re-attaching symmetric dimensions
===Translators===
PR 8957904: Line missing in dxf when using save as flatten
===API===
PR 8954367: Exception on close in visual.dll when using SEPreview.ocx
PR 8949119: Tube.Path(objNPaths) throws an exception in ST9
PR 7993126: ST9 custom addin menu is devided two tabs using API of AddCommand.
===General===
PR 8333251: user-specific paths cause saving problems after deploying sepref to another user
PR 7925571: Performance for Open new Part/PSM/ASM is SLOW
PR 8901488: New revisions for all FOP members are not replaced in assembly in below workflow
===Insight===
PR 8900552: Asm cfg can't be saved and other strange behavior after use of Save As Copy
===Teamcenter Integration for Solid Edge===
PR 7767962: The last_released_status property does not map correctly in SEEC
PR 8957604: SEEC: Item Number column in Occurrence Properties disappears
PR 8919610: SETranslationsServices generates application error while converting dft to pdf
PR 8934757: AtT: Stops functioning when selecting different group roles via cache
PR 8945903: SEEC crashes when opening FOA from MRU after new member created
PR 8945903: SEEC crashes when opening FOA from MRU after new member created
PR 8917637: SEEC: Project Name displays Item Name instead of actual value for Project Name
===Built-in Data Management===
PR 8937432: Unregister SEPropertyhandler.dll, windows event log does not capture the process
===Design Manager===
PR 8902403: Design Manager: Unexpected overwrite message is shown during Save As
PR 8947721: Where Used process crashes with a Close Program error when selecting Recursive
PR 8886062: Design Manager with Insight don't maintain the column setting
PR 8901842: ST8 aborts using Property Manager
===Mold Tooling===
PR 8894127: Associative with Material is unchecked at Material Dialog reopen.
09-15-2017 02:39 AM
Readme file says:
Microsoft Installer (MSI) Maintenance Pack
Product: ST9 MP9
Version: 109.00.10.04
I guess it is a copy paste forget
09-15-2017 05:31 AM - edited 09-15-2017 05:37 AM
Fast Search is still not working after MP10 installation. Do I need to re-register the dll manually?
I installed the MP as administrator but I'm using SE as regular user, may be this could be the reason for the forgotten registration of the DLL? I don't know if this DLL work in user-space or for all-users.
09-15-2017 05:45 AM
@Alessandro wrote:Fast Search is still not working after MP10 installation. Do I need to re-register the dll manually?
I installed the MP as administrator but I'm using SE as regular user, may be this could be the reason for the forgotten registration of the DLL? I don't know if this DLL work in user-space or for all-users.
Fast search were fixed with MP9 but with a separate update file (Fast_Search_MSI_MP9.exe)
Do you mean with MP10 it's broken again ?
09-15-2017 05:54 AM
After MP 10 installation the fast search feature does not work, but I didn't tested if it worked before installation. I'm sure it worked a few day ago with MP9 installed, but a big Windows update happened in the meanwhile.
At least the MP10 installation didn't fix the problem, but it is also possible that it broke something that worked before MP10 installation. It is also possible that the responsable is the last windows update too.
I registerd the DLL as regular user but with no success. After that, I did it as Administrator and now Fast Search works again, I guess until the next rain in the other side of the world...
09-15-2017 06:22 AM
@Alessandro we have just been made aware of a particular issue with MP10 Fast Search on Windows 10. This issue is not widespread and does not reproduce on all Windows 10 systems. We are actively investigating this issue now.
Please contact your Solid Edge support person and submit an IR to GTAC. In your IR please reference existing PR 8978423.
Again, this is not occurring for all systems and at this time appears to be limited to only a few select systems.
09-15-2017 06:23 AM
@Alessandro P.S. When you get your IR submitted to GTAC please PM me the IR number and I will actively pursue getting this moved forward for you.
09-15-2017 12:02 PM
@uk_dave, can you share the symptoms of this issue?
09-15-2017 12:11 PM
@KennyG for the particular issue reported in PR 8978423, after installing MP10, the out-of-the-box Solid Edge properties are then missing from indexing but any custom properties are still being indexed. Re-registering the dlls [as with most indexing issues] should resolve the issue.