Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 11 Announcement

Siemens Legend Siemens Legend
Siemens Legend

October 20, 2017


Dear Solid Edge Customer:


Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 11 is available for download.



The Solid Edge Team




Release Notes:



Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.



Update Version:




Download Location:



ST9 Maintenance Packs can be downloaded from:






Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.


  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.


  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.


  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.


  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.


  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.


  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.


  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.


  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).



E-mail Notification:



To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail



For details on initiating your email subscription navigate to:



This Maintenance Pack addresses the following PRs:



===Part/Profile/Sheet Metal===

PR 8920032: Part Painter: New Face Color will only show after a feature recompute

PR 8959244: Can't Dimension Live Section

PR 8962282: BlueSurf edit terminates SE

PR 8967458: Sketch Dimension in ST8 is locked, while in ST9/ST10 is unlocked

PR 8928360: Problem mentioned in PR as "Report font size gets larger when creating a report." is fixed.

PR 8975910: Edge crashes when changing material properties.

PR 8986120: Lack of properties after Save as of Template file.

PR 8994736: Material Table Import does not read Excel files



PR 8856499: Occurrence property overrides are incorrect when obtained from automation

PR 8920113: SE-User defined mass not carried into upper-level assembly



PR 8854778: Paper Print > Print Preview > Current Display is wrong

PR 8966926: A filled area is not displayed correctly in ST9

PR 8968657: Excel's title inserted in Draft file.

PR 8965535: User-defined mass for frames is not correct in a parts list.

PR 8965910: Position of dimension moves, when opening ST4 draft in ST9.

PR 8981098: Fixed a problem where sectioning was failing in certain cases.

PR 8984946: Tolerance Table does not work for smart dimensions along 2 edges

PR 8985069: Broken view becomes un-broken when opened in ST9

PR 8985129: The border of callout disappears when opening the data of ST4 in ST9.

PR 8997929: Nail board is not constructed properly



PR 8938055: Dimensions spanning a Broken View are incorrect after translation to & from DWG

PR 8902860: Callout is moved after save as dwg.

PR 8977298: Text in block in background sheet moves incorrectly during translation.



PR 8805700: The background of the icon added by the add-in does not become transparent.


===Teamcenter Integration for Solid Edge===

PR 8975742: Enable TcServer Logging at SEEC Login

PR 8944560: Where-Used folders showing red when mapping to fully qualified name share

PR 8989513: Crashed while searching ANSI ASM template and open it.

PR 7767962: The last_released_status property does not map correctly in SEEC

PR 8994811: Copy and paste from AWc to Asm does not work


===Built-in Data Management===

PR 8964054: Problem with Where-Used (BIDM) - does not work permanently

PR 8978423: Fast Search: SE Properties are lost after applying ST9 MP Patch


===Design Manager===

PR 8932196: Save as does not remain in the last selected folder location


Fred White
Siemens PLM Software