Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 12 Announcement

Siemens Legend Siemens Legend
Siemens Legend

November 20, 2017


Dear Solid Edge Customer:


Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 12 is available for download.



The Solid Edge Team




Release Notes:



Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.



Update Version:




Download Location:



ST9 Maintenance Packs can be downloaded from:






Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.


  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.


  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.


  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.


  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.


  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.


  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.


  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.


  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).



E-mail Notification:



To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail



For details on initiating your email subscription navigate to:



This Maintenance Pack addresses the following PRs:



===Part/Profile/Sheet Metal===

PR-8993184 & 8991276: Solid Edge crashes when select a face to extrude in synchronous mode 

PR-8000869 Solid Edge freezes while sketching 

PR-8993927 Parasolid file crashes Solid Edge when opened V109

PR 8935713: Max path length of file location



PR 9009522: Physical Property Manager shows different results vs Physical Property Dialog

PR 8944800: Differing Physical Property dialog values based on the level the assembly was opened



PR 8987166: Print problems with shaded views



PR 8997333 AutoCAD translation issue -Text location changes



PR 9009806 Wrong title displayed in Excel in this workflow



PR 8999431 The behavior of the shortcut key is incorrect


===SE SP===

PR 8346838: BOM Reports are missing files


===Teamcenter Integration for Solid Edge===

PR 8992417: Properties in Property manager are locked when file have a TC Status assigned


Fred White
Siemens PLM Software