Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 13 Announcement

Siemens Legend Siemens Legend
Siemens Legend

January 30, 2018

 

Dear Solid Edge Customer:

  

Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 13 is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.

 

=============

Update Version:

=============

 

109.00.13.03

 

================

Download Location:

================

 

ST9 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.

 

  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail

notification.

 

For details on initiating your email subscription navigate to:

http://support.industrysoftware.automation.siemens.com/general/email.shtml

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 9008679: GetLengthAtParam() throws unspecified error

PR 9007760: Call to API methods in custom AppDomain not working as expected

 

===Part/Profile/Sheet Metal===

PR 8981720: Recompute lets features fail - part is destroyed

PR 8997613: Item Type Property mapping error from Solid Edge Standard Parts to Teamcenter for standard parts

PR 9008477: Layer behavior in part and assembly sketches after creating a block

PR 9043412: XpresRoute gives an error when using saved setting end treatment of 90 deg

 

===Assembly===

PR 8993495: Reference plane does not update when linked excel variable changes

PR 9023839: Deleting a relationship aborts in DCM code

PR 7601296: Physical properties, update on file save does not work

PR 9034045: Sketch drawn in SE assembly is not displayed upon exiting from sketch environment

                                                                                                                                                          

===Draft===

PR 9009961: A modification that succeeds in MP9 ends into errors in MP10

PR 9016318: Broken out section doesn't cut disjoint bodies correctly if there was no intersection with a solid region

PR 8957087: Coordinate dim on rotated view is incorrect

 

===General===

PR 8536218: Saving SE files when there is no disk space results in data loss

PR 9018172: Menu / Icon load slow after installation of Windows 10 Fall Creator Update

 

===Insight===

PR 8956565: Insert assembly copy does not allow me to create new mirrored parts

 

===Teamcenter Integration for Solid Edge===

PR 8950787: Open dialog Files of Type field changing

PR 8970920: PDF is checked out in TC and save of draft gives non related error

PR 8989772: No SE save_prompt closing asm after changing occurrence property via API

PR 9013888: SE Status User Display property not changed when status updated via automation

PR 9053765: Add to Teamcenter - Interactive, Item Name / Title mapping problem

PR 9062383: Mass is changing from lbm to kg when saving into TC

PR 9030895: XpresRoute failures; no Material and error displayed

PR 9031327: CPD does not get updated with change in Item selection

 

===Translators===

PR 9004389: Abort when trying to open DXF Files

Regards,
Fred White
Siemens PLM Software
7 REPLIES 7

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Legend
Legend

Anyone knows when ST10 MP4 comes out?

 

Friday my company moves over to ST10 and we would like to take PR 8981720 (Recompute lets features fail - part is destroyed) fix with that Man Happy.

Sander
The Netherlands

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Valued Contributor
Valued Contributor

Hi,

 

see Laura's yesterday post here.

 

SE2019 MP3

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Siemens Legend Siemens Legend
Siemens Legend

@Sander-NL We had an original target date of 5-FEB. However, we held the last build up a bit to allow one additional PR to be checked in. The late PR arrival incorporated a code workaround to resolve a problem introduced by the Windows 10 Fall Creators Feature Update. With that, the new target date for ST10 MP4 is 12-FEB. 

 

The PR you mentioned is on the list of PRs to be verified in MP4.

 

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Legend
Legend

Thank you for the information.

 

As we are working on ST8, it will still be a improvement Smiley Wink.

Sander
The Netherlands

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Experimenter
Experimenter

Link is not working. Could you please update the link for ST9 maintenance packs?

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@DaviNEC  All Maintenance Patches for versions prior to ST10 have been removed from the download site.  Not sure why, but that is the reason the link no longer works.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST9 - Maintenance Pack 13 Announcement

Experimenter
Experimenter

Hi Ken (@KennyG), thanks for the prompt reply. Best regards. Davi