Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 3 Announcement

Siemens Legend Siemens Legend
Siemens Legend

November 28, 2016

 

Dear Solid Edge Customer:

  

Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 3 is available for download.

 

Sincerely,

The Solid Edge Team

  

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked as Installed Updates.

 

================

Download Location:

================

 

ST9 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.

 

  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 7820176: Solid Edge Crash on calling GetCharStrokedCurveData() API on Stick Font

PR 7859975: Problem with the API 'ContourFlange.UseGlobalBendRadius'

PR 7864711: SEEC FileProperties CheckOut

PR 7812938: RevisionManagerAction.ReleaseAction does not accept new path

PR 7852881: API, PMI objects to be added to the Flat Model PMI section

PR 8318016: Commands moved to Backstage not being enumerated by CommandCategories API

 

===Assembly===

PR 7796044: Engineering Reference gives wrong results for Worm Gear parameter of Gamma angle

PR 7802414: Pattern occurrence entries not highlighting when pattern first expanded

PR 7813587: Open All Hidden followed by Show All not displaying all components

PR 7761781: Solid Edge hangs while updating spur gear

PR 7846369: Display anomaly on selection after rotating assembly

PR 7819588: Some file properties are deleted when using create in place

PR 7535165: Profile not flipping direction based on variable modification

PR 7847434: Problem with wiring harness aborting

PR 7866584: Misplaced Custom Piping components

PR 7869943: Changing a value in the variable table displays units

PR 7856808: SE crashes when component is dragged in the assembly

PR 7822141: Replace face with Sync if possible not rolling back to ordered features when complete

PR 7852435: During Create Part In-Place the CS 'Z' axis not always aligned correctly

PR 7852428: F4 lock is not honored when placing origin at center of radius

PR 7787450: adjustable assembly does not solve correctly

PR 7863988: Lower Pathfinder disappears after changing background in Part Edit environment

PR 7869402: Crash when creating a bundle in wire harness on Windows 10

PR 7535254: Parts List Item number changes in an Insight revise workflow from Draft

                                                                                                                                                          

===Draft===

PR 7781203: Exporting to DXF move Tables to layer 0

PR 7781877: A balloon becomes NA in ST8

PR 8314032: Wrong Sheet number position on Printout (Sheet number / Number of Sheets)

PR 7845791: Angular coordinate dimension behaves incorrectly

PR 7799589: automatic centerlines on section view always detach on update

PR 7808285: Problem moving a smart dimension after loading ST8 MP10

PR 7810320: Style Organizer browse dialog always defaults to the Materials folder

PR 7862290: Crash after copying fill style with Style Organizer in German ST9

PR 7821095: There is a difference in active view and inactivate view in ST8

PR 7852191: When aligning a sheet metal flat pattern by key points, break line projection is broken

PR 7864528: Coordinate dimension line just keeps on extending

 

===Part/Profile/Sheet Metal===

PR 7849980: Internal errors when executing the close corner command

PR 7820757:  'New Filename' has empty values for the Excel entries when doing a 'Save As'

PR 7812225: Edit of include with offset results in loss of associativity

PR 7742649: Updating mirrored features is not triggering update on multi-bodies

PR 7854086: Out of date property gets updated after adding custom property in this case

PR 7859191: Keypoint Curve not working as expected in ST9

PR 7868432: Cannot pattern a feature from feature Lib, but could with ST8, regression

 

===General===

PR 7821956: Buttons not shown on Cloud Enabled Gateway for non-English installs

PR 7758300: Cloud Enabled user not able to start SE on 1st machine after logging off 2nd machine

PR 7850243: MRU thumbnail not scaled properly

PR 7857892: ST9 Revise is causing drawing files to be named incorrectly 

PR 7860390: Solid Edge closes when using custom theme on Windows 10

PR 7877292: SEAdmin Settings and Preferences browse issue

 

===Design Manager===

PR 7814031: Design Manager / LCA does not show the Filenames only Icons

PR 7794682: Incorrect copying the file name using the keyboard shortcut in Design Manager

PR 7853010: Save As from Design Mgr with LCA on is incorrect

PR 7857747: User is able to revise part having parent with In-Work status by another user

PR 7858014: Revise and Save As perform should behave consistently

PR 7821545: Error seen on running duplicate report.exe by non admin user

 

===Insight===

PR 7808341: Insight/SharePoint mismatch with cfg file

PR 7874100: Cache not updating causing loss of work

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7858234: Manage tab disappears after deselecting SharePoint

PR 7815064: Sort in SESP Parts Library difficult - Column Title line overlapped

PR 7823490: Assembly crashes when adding parts

PR 7782224: Actions are unavailable hence unable to design custom workflows

 

===Teamcenter Integration for Solid Edge===

PR 7818037: Virtual Components issue

PR 7852179: Structure editor after an itemid paste operation appends a "_1" to the filename

PR 7799064: Teamcenter runtime errors checking in SE files

PR 7845687: Crash when working with draft and assembly files in Teamcenter 10.1.6

PR 7868471: The new workflow process access from SEEC is incomplete

 

===Translators===

PR 7817678: upload all option not working as expected in multicad assembly in managed mode

PR 7817397: Problems to export a simplified assembly to Parasolid 24.1

PR 7817771: STEP-Export: Parts missing

PR 7867329: Error when check in of assembly in certain circumstances

PR 7871611: Active Workspace pane is not showing when connecting via 2-Tier

PR 7872464: Need more automation support to drive date in the SESE grid

 

Regards,
Fred White
Siemens PLM Software
11 REPLIES

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Hi Fred,

 

Any word on whether MP3 will fix the problem of Design Manager not being able to launch using right click.  I posted an issue where an error message of "there was a problem sending the command..." ?

 

 http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/ST9-Problems-with-Design-Manager/td-...

 

It's reported under IR7809269

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Siemens Legend Siemens Legend
Siemens Legend

Hi Kyle, 

 

Sorry, no solution in MP3. This problem is being tracked by Master PR 7803803.

 

I have escalated the problem for review in our next Change Control Board meeting requesting the PR be investigated for ST9 MP4. There are currently 4 customers reporting this behavior.

 

Once scheduled for investigation, we may need to request a few more machine specific details on the machine you are reproducing this problem on. Thus far development has not uncovered a combination that will reproduce the issue each time so it can be captured in the debug environment.  

 

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are the Insight Server MPs not uploaded yet?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Hi Fred,

 

Ok.  I can launch DM separately and run it in that manner for now.  

 

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Siemens Legend Siemens Legend
Siemens Legend

Hi Bruce,

 

Yes, both 2010 adn 2013 Insight Server MPs are posted:

 

Untitled.jpg

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm getting a "Permission denied" message when I click on the Insight Server/ folder.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Siemens Legend Siemens Legend
Siemens Legend

Sorry Bruce.

 

It appears I put a space in the folder name. I have renamed the folder now - Insight_Server. Give it a bit to sync with the other FTP servers and you should then be able to access the folder. 

 

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Phenom
Phenom

In order to roll back a maintenance pack, would we need to have installed earlier ones, or do we simply have to have the earlier MP available ?

I ask because we haven't yet updated to ST9 (or even ST8), but when we do we don't really want to install several MP's.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Solid Edge ST9 - Maintenance Pack 3 Announcement

Siemens Legend Siemens Legend
Siemens Legend

MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2. Therefore, when you move to ST9, you can install the latest MP available and get all fixes.

 

MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall). The current MSI Product Update will be the only Update listed and available for uninstallation. After the current Update is uninstalled, the previous Update will become the current Update. Example: If you have installed MP1, MP2, and MP3. Removing the current Update will revert you to MP2, and so on. If you only install MP3, removing the current Update will revert you back to the base release. 

 

Regards,
Fred White
Siemens PLM Software