Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 4 Announcement

Siemens Legend Siemens Legend
Siemens Legend

January 24, 2017

Dear Solid Edge Customer:

Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 4 is available for download.

Sincerely,
The Solid Edge Team

============
Release Notes:
============
Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked as Installed Updates.

 

================
Download Location:
================
ST9 Maintenance Packs can be downloaded from:

https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/

==========
Installation:
==========

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be
uninstalled using Uninstall a program from the Control Panel.

• MSI Product Updates can be applied on top of the base release and or existing Product Update
with a lesser version.

• MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered
in MP1 and MP2.

• MSI Product Updates calculate free disk space before installing. Please note that there have
been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

• MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

• Uninstalling a MSI Product Update will restore the installation to the state before the Product
Update was applied.

• PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous
Product Update package, if any, must be available to allow the recovery of previous file versions.

• The current MSI Product Update will be the only Update listed and available for uninstallation.
After the current Update is uninstalled, the previous Update will become the current Update, if
there were multiple Updates installed.

• MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed
updates -> Uninstall).

===============
E-mail Notification:
===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

=========================================
This Maintenance Pack addresses the following PRs:
=========================================

===API===
PR 7900912: Problem with 'GetCharStrokedCurveData() API for Stick Fonts

===Assembly===
PR 7852674: Problem with insert assembly copy in ST9 with our Add-In
PR 7864653: Valves are not found for placement even available in library
PR 7881633: Fixes for random crashes captured in crashlogs
PR 7890629: Fixes for random aborts reported by crashlogs when placing parts in an assembly
PR 7894935: Flange is moved after splitting a line in a Pipe-Route
PR 7904106: assembly not opening in ST9
PR 7626749: abort when deleting and then creating new assembly relationships
PR 7885640: wrong mass in property manager solution
===Draft===
PR 7883790: Zoom area cross hairs are white on draft
PR 7894371: Incorrect thread depth line
PR 8316956: Overlapping dimension text when importing
PR 7890502: Handle in projection line in dimensions doesn't work properly
PR 7895426: Filled arrow of dimension isn't filled after MP3
PR 7895600: Symmetric Diameter reattaches abnormally
PR 7901853: Reattach dimension fails initially using customer's Dim Style
PR 7882876: Break lines are difficult to locate
PR 7909444: Draft Balloon issue in MP3
PR 7883816: Drawing view (hatch/fill) rendering problem while zooming IN/OUT
PR 7897801: When importing DXF, background of A2-sheet is always used

===Part/Profile/Sheet Metal===
PR 7809829: Solid Edge closes clicking on empty field in Function name window
PR 7821896: Change formulas in Dynamic Edit
PR 7848269: Material table file is not showing in the Material Table dialog
PR 7872669: Fully positioned sketch change position after modifying dimension value
PR 7883754: Deleting materials in material table crashes Solid Edge
PR 7871739: large assembly performance and "filter/grate" sheet metal
PR 7880891: Switch from shading to tessellation, while measuring, reproducible
PR 7891594: Moments of inertia axis are clearly wrong with multiple areas
PR 7898222: NX Nastran solve error: element refers to an invalid property entry
PR 7900945: Factor of Safety is wrong for both parts because it is based on Steel
PR 7907104: Crash when trying to create assembly report, W10 only
PR 7868958: Dependent features fail after inserting feature library

===General===
PR 7821669: Replace part (psm) dialog box defaults to "Top Level Assembly"
PR 7875367: Crashing repetitively when starting the property manager
PR 7907120: Problem entering drawin in view in draft in MP3
PR 8318016: Same command list being returned for all categories
PR 7891664: SECopySettingsWizard.exe does not deploy registry setting correctly
PR 7923212: SE Performance slowed down with 3D Connexion add-in enabled

===Design Manager===
PR 7859140: Already released documents will be moved again to a wrong folder
PR 8318098: Design Manager hangs during Search in Where used results for ".dft"
PR 7859146: Design Manager will use a wrong folder when an InWork document will be revised
PR 7914404: Deselect action performance is poor compared to ST8
PR 7807876: Replace in Design Manager does not detect texts that were already replaced

===Built-in Data Management===
PR 7815252: Where used finds only one draft of two

===Insight===
PR 7858933: Problems with revise function from Solid Edge
PR 8322281: SolidEdgeInsightParser creates Custom Properties for properties not DocLib Colum
PR 7883052: Parts missing when opening an assembly deactivated/simplified and switching to design

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===
PR 7764855: Update Drawings doesn't update (generate) PDFs
PR 7792386: Origination date is incorrect if revise with is done via Solid Edge or Web interface
PR 7866126: Standard Parts icon disappeared from SESP Parts Library in ST9
PR 8311586: UpdateCallouts.exe fails with Unknown Error

===Teamcenter Integration for Solid Edge===
PR 7799064: Teamcenter runtime errors checking in SE files
PR 7850576: Material value of part not retain when performing Save As of related draft
PR 7888907: Qualifier /master=cad does not work
PR 7817678: upload all option not working as expected in multi-CAD assembly in managed mode
PR 7878977: Root Folder not allowed in Search
PR 7884341: Selection of LOV value in SEEC upload delivers wrong result
PR 7897204: Save As of assembly results in error "Child not found for delete"
PR 7909284: Different Open workflows produce different results
PR 7910203: Propseed.txt set in Options.xml is ignored
PR 7910238: Custom Property Type/Typ is not working with Teamcenter
PR 8322981: SE templates management is not possible by user other than infodba
PR 7896574: SE crashes while opening assemblies from SEEC

===Translators===
PR 7890094: Import Parasolid will not import complete geometries, only in Part-environment
PR 7890357: DXF export translator doesn't translate properly text scale in callout

Regards,
Fred White
Siemens PLM Software
2 REPLIES 2

Re: Solid Edge ST9 - Maintenance Pack 4 Announcement

Experimenter
Experimenter

Hi There - 

 

I have solid edge ST9 academic version. I am having a host of issues with it crashing / not performing as intended so I'd like to install this maintenance package. I am trying to get a "WebKey" account setup, however I don't know my "Sold-To-ID" since I have the academic version. How can I find it or is there a work-around? 

 

Thanks much

Nick Beers

Re: Solid Edge ST9 - Maintenance Pack 4 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you got it through a school (you did not download from Siemens the "Student Version") your school administrator can get you the Maintenance Patch.  If you have the Student Version downloaded from Siemens, then you will not have access to the Maintenance Patch.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com