Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid Edge ST9 - Maintenance Pack 5 Announcement

Siemens Legend Siemens Legend
Siemens Legend

March 21, 2017

 

Dear Solid Edge Customer:

  

Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 5 is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.

 

================

Download Location:

================

 

ST9 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.

 

  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail

notification.

 

For details on initiating your email subscription navigate to:

http://support.industrysoftware.automation.siemens.com/general/email.shtml

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 8324311: Exception when PatternOccurrence is selected

PR 7950084: UseGlobalBendRadius is not modifying the CF feature's to use global bend radius

PR 7936594: A parts list update was incorrect if assembly loaded

PR 7962044: GetCharCurveCount API returned 0 curves for some characters

PR 7955506: Cannot Add SheetMetalGage Property through API

PR 7816060: Frequent crashing in JAsmTube::ImpIJAsmTube:Smiley FrustratedetMaterial

PR 7948804: Changing gage through API is not updating the bend radius values

 

===Assembly===

PR 7812286: Custom part is added in standard part library but cannot call through Piping

PR 7918004: Solid Edge crashed while moving the part with copy option and tangent constraint

PR 7919175: Drag with copy option is working differently IPA'd -vs- Opened

PR 7898132: Case-specific crash when deleting a part from assembly

PR 7892218: Cannot change occurrence properties settings in this assembly

PR 7939113: RMB on pathfinder during edit in place of a feature doesn't work

PR 7920864: Fixed a crash identified by auto crashlog capture

PR 7922996: Solid Edge is crashing after creating wire harness

PR 8528424: Solid Edge is crashing when reopening this assembly file

PR 7938545: MRU Thumbnail not show for alt assemblies

PR 7967585: Solid Edge keeps crashing randomly

PR 8327420: Crash when exiting sketch after placing a block

PR 7969451: Abort in relationship tree when selecting a certain relationship

PR 7972055: Solid Edge crashed when applied sensors - Win 10 specific

PR 8323188: Frequently crash working with Solid Edge

                                                                                                                                                          

===Draft===

PR 7783355: Crash when updating views on a file with missing component

PR 7886994: DWG is not correctly translate with Solid Edge

PR 7908506: Can't Attach/Detach radial dimensions using Alt + drag

PR 7920509: Breakline creation fails if keypoint is selected from previous region

PR 7918120: Aspect ratio of sheet changes as length exceeds 109.22 inch

PR 8324292: Dimension lines of Angular Dimensions are imported much too large

PR 7789711: Changing scale of view does not change scale of principal view with break lines

PR 7904338: Dimension style doesn't preserve Annotation-connector line type

PR 7931370: Dimensions deleted when centerline is moved

PR 7946095: Windows re-indexes all items after installing SE

PR 7944009: SE crashes when moving an aligned and grouped drawing view.

PR 7958506: Balloons don't update after changing item number via put_ItemNumber

PR 7928057: Dimensioning detail views

PR 7937124: Cannot get reference key for silhouette edges

PR 7945104: Column with multiple property texts is not sorting correctly

PR 7970209: ST8 draft file aborts when opened in ST9

PR 7945679: DV/PL do not go OOD when user adds/removes occ property overrides

 

===Part/Profile/Sheet Metal===

PR 7926588: Solid Edge crashes after getting area of sketch

PR 7858006: Cutout will stop if dynamic preview is OFF

PR 7889432: Unable to Delete imported Wireframe without hiding first

PR 7901408: Link to material leads to a crash on update

PR 7920601: Variable values in ST9 Ft-In 0 is not there

PR 7868004: summary of atomic parts shows assemblies

PR 7928935: The Subject is not available in the tab Details of the properties on the OS

PR 7931593: Auto dimensions are getting marked as in error

PR 7940215: Tear-off command crashes Solid Edge

PR 7938629: Crash at 'JMSetManager::AddToSubsetWithSameMpartOwner'

PR 7915615: Unable to select copied sketches with manipulation commands

PR 7916470: Drag and drop is not supported on simulation studies

PR 7929149: Performance time increase when applying material to a part

PR 7940333: Solid Edge crashes when sectioning the extrude feature

PR 7920410: Solid Edge crashes editing a component of an assembly

PR 7939535: Cannot flatten sheet metal of Part-Copy

PR 7945373: Normal Cutout Thru All gives failure warning even though it succeeds

PR 7904897: save file causes a 'cannot access file' message... 2 times out of 3 when saving to a server

PR 7913897: API Exception when hole collector will be selected instead hole features

PR 7908712: The shape of Flat Pattern is incorrect. Please correct in SE ST8 MP

PR 7959342: Flat Pattern will not be created correctly

 

===General===

PR 7858083: Incorrect behavior when user defined templates exceed sixteen files

PR 7892075: Creating new theme with commands in QAT results in slow sketch lines

PR 8313169: Path for 'User templates' does not update in 'Fast property search'

PR 7892297: Cannot create the folder c:\Users\User B\Appdata\ when starting Solid Edge

PR 7939613: Custom program using SEDraftX.ocx results in blank buttons

PR 7913560: Solid Edge is crashing frequently...Crash logs for Dev Review

PR 7666914: Defining keyboard-shortcuts will mess up configuration

PR 7925373: Further File Open and File New performance improvements

 

===Design Manager===

PR 7849732: Design Manager tries to rename the folder path

PR 7940999: Design Manager duplicate file name error indication

 

===Built-in Data Management===

PR 7905132: Fast search, Search tool does not work if "Look in folder" use a mapped drive

 

===Insight===

PR 7928903: LCA Error Message with strange characters for checked out documents

PR 7882183: Parts not displayed when asm will be loaded as simplified and then as designed

PR 8325252: Parts not displayed when asm will be loaded as simplified and then as designed

PR 7886563: Released Documents can't be moved back to available

PR 7870628: LCA's apply status to linked documents option not using the options.xml.

PR 7939490: Property Manager removes all material definitions in French version

PR 7972514: Material change with Phys. Property Manager clears materials for parts

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7930745: CPD column widths continually increase each time an upload/check-in is performed

 

===Teamcenter Integration for Solid Edge===

PR 7884971: Create a draft from part while showing vertical prop window errors

PR 7915586: Custom Property in SEEC File Properties has limited string value

PR 7921892: Update of Property Text in SE Draft requires opening model file

PR 7926338: Modify value in CPD master=cad property does not change attribute in RAC

PR 7803149: Add to Teamcenter Interactive crashes when using the function "Find all related Drafts"

PR 7927588: Customer has some family of assemblies where the API to list properties in ST9 is very slow

PR 8326383: NULL value is not sync'ed with /master=cad

PR 7866423: Canceling the Login menu with custom template list active forces multiple cancel

PR 7875837: Add to Teamcenter crashes

PR 7891459: Problem with Attribute Mapping on SE Draft

PR 7916950: Add to Teamcenter Interactive does not accept 'units' in Density attribute

PR 7927661: German Callout for Filename is not working correctly

PR 7921740: Save As, if the project is cleared then cancelling project dialog re-populates

PR 7925504: Multiple crashes when editing blocks, crash occurs in EditBlockView

PR 7945874: Check In All cause BOM view crash

PR 7948241: Save As from SE Draft loses Material already assigned to original Part Rev

PR 7950067: Drawing views linked to SE Draft Dataset from same Item Rev

PR 7957318: Non-graphic Parts in SEEC and Teamcenter not working with ST9

PR 7958783: “Teamcenter has defined unique Item Numbers" due to Alt Pos Assy usage

PR 7966653: JT Part Properties are populated to Solid Edge Assembly Properties

PR 7977369: Copying a JT-component in SE Assembly does not trigger SEEC BOM

PR 7992576: Replace Part command is not working for JT-based Driven References

 

===Translators===

PR 7787919: Error of translating to IFC with enabled option 'Export displayed only'

PR 7929985: ST9 can’t open STEP file

PR 7907191: When exporting draft files to AutoCAD, the unwanted line weight now shows up

PR 7915468: Getting Error "The migration has been terminated"

 

Regards,
Fred White
Siemens PLM Software
21 REPLIES 21

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Gears Phenom Gears Phenom
Gears Phenom

YEAH! It fixed the Fast Search templates location.  Now all my properties can be indexed!


____________________________________
--Scott Wertel, P.E.

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Gears Phenom Gears Phenom
Gears Phenom
"PR 7945373: Normal Cutout Thru All gives failure warning even though it succeeds"

Weird, I just noticed this started this past week..Guess I'll see if does resolve the issue.

-Craig

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Already I have two issues that are problems with this maintenence pack. The very first 2 things I attempted to do. I immediately filed an IR for the first, but I don't have time to do so with the second.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Any chance you might share what those problems are?  Cheers!

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@nominus38  Can you mention what the 2 problems concern? I may not want to install the MP if they'd be problems for us.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Gears Phenom Gears Phenom
Gears Phenom

(view in My Videos)
The first has to do with inserting a part copy into a psm file, if you have the option to match the material it gives an error that no part body or whatever can be found. It's already been converted to a PR as it was duplicated immediately. The other problem I noticed is in an assembly, when I try to drag another component into it from windows explorer, it just acts weird and never brings the part or subassembly in. Doesn't happen if I bring it in using the part library function in Edge, only when bringing in from a windows explorer window.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks. No worries for me with those two. Let's hope there are no others.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Honored Contributor
Honored Contributor

Wow, that's alot of issues fixed.

 

But being able to drag and drop from windows is a big one for me. I do everything that way. My design environment is too fluid for anything else. 

 

I will have to hold off until I have enough time to uninstall if there are problems. Fast projects the next few weeks. 

Re: Solid Edge ST9 - Maintenance Pack 5 Announcement

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I just tested drag'n'drop from Windows Explorer and it seems it works fine.

Tested on 2 machines with ST9MP5 and Win10.

 

Can somebody check this on Win7?

 

Ota