Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 7 Announcement

Siemens Legend Siemens Legend
Siemens Legend

May 22, 2017


Dear Solid Edge Customer:


Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 7 is available for download.



The Solid Edge Team




Release Notes:



Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.



Download Location:



ST9 Maintenance Packs can be downloaded from:






Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.


  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.


  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.


  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.


  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.


  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.


  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.


  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.


  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).



E-mail Notification:



To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail



For details on initiating your email subscription navigate to:



This Maintenance Pack addresses the following PRs:




PR 8815887: User is unable to apply exploded configuration through API

PR 8815859: User not able to get/set assembly occurrence style/facestyle via automation

PR 8007055: ImportStyles2 API errors when try to import text styles for par and psm files



PR 7587419: Crash when deleting or applying a display configuration

PR 7960971: Simple Fillet weld fails in ST9, works in ST8

PR 8816727: SE Crashes while replacing parts in a subassembly that we cannot grab write access to



PR 7921364: Performance regression updating views due to Parasolid

PR 8002331: Draft file goes into continuous processing trying to delete table

PR 8802422: Issue when transitioning to a draft document

PR 8804601: Solid Edge crash when opening a draft file since ST9MP5

PR 8805898: Crash when trying to create a block with table in block edit/open environment

PR 8812228: Wrong visualization when dragging (fast) the draft 

PR 7977163: 2D Model View not placed at the lower left hand corner of the Draft She

PR 8815632: Dimensions lost after arranging

PR 8834164: Dimension Prefix: focus erases previous entry


===Part/Profile/Sheet Metal===

PR 7939432: Decreasing Performance from ST7 to ST9

PR 8000330: Update to ST9 from ST5 - Many errors in parts after transition.

PR 8331522: Exporting DXF through workflows results in empty dxf

PR 8805044: Wrong mouse focus in "Material Table", Face Style gets changed

PR 8000330: Update to ST9 from ST5 - Many errors in parts after transition. - V109

PR 8004081: Error "Design Body cannot be found" inserting part copy w/material duplicate on.

PR 8805393: Variable is not captured correctly when selected from the screen

PR 8815166: PMI does not work properly, cannot create driving tangential dimensions

PR 7964860: XpresRoute - tubes cannot be deleted

PR 8826705: Through next option in hole dialog should be disabled

PR 8807712: Hole missing in dxf after save as flat

PR 8818016: Reports give wrong values for Parts in a subassembly.

PR 8824475: Unable to edit sheet metal thickness if Enclosure feature created for model



PR 7872381: Solid Edge UI fails when a mobile phone is plugged into PC

PR 7939268: Properties in Win explorer will not be shown as was in ST8

PR 8808278: Options.xml, file naming rule will not revert to none


===Design Manager===

PR 8322507: Revising of an Assembly with Draft the draft skips the next revision


===Built-in Data Management===

PR 7958078: In built data management issue, not available in Foundation



PR 8328877: Parts not displayed when asm will be loaded as simplified and then as designed


===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 8807966: Manual naming produces _1 at the end of file

PR 8833313: User is not able create revision for FOA


===Teamcenter Integration for Solid Edge===

PR 7978442: Problem with multiple revisions using rules Latest by creation date and Precise

PR 8817237: Draft Filename gets cryptic value on Revise

PR 7997393: Prop Seed values result in odd character displayed in properties dialog

PR 8334013: offer SE Draft template if empty item with BVR is open from TCRAC

PR 8334357: Wrong JTposition of assembly features after saving in ST9

PR 8818805: Replace Part with Copy from SE Asm loses Material from the original Part

PR 7938494: FOA custom property mapped master=both reverts to old value after save

PR 8806327: Mirror Component fails in SE Assembly - see error

PR 8817943: Problems with « New » shortcuts when logged in Teamcenter

PR 7969903: Edge.exe not releasing memory after repeated open/close of Assembly file

PR 8806327: Mirror Component fails in SE Assembly - see error

PR 8817943: Problems with « New » shortcuts when logged in Teamcenter

PR 8833954: Type ahead on Project ID dialog in the CPD changes name of project

PR 8828094: jt overrides not uploaded if 2 assemblies on CPD

PR 8818363: Take Ownership command disabled for top level Asm

PR 8828843: SESE crashes trying to change projects



PR 7959741: Dxf Out: Hatch within a trimmed (Spline) Section View will be exported untrimmed.

PR 7997794: DWG Import doesn't create sheets and sheet geometry - AutoCAD Model is empty

PR 7847907: SW 2012 Data migration does not create associative drawing

PR 7911065: Solid Edge crashes when importing a Parasolid in assembly template


Fred White
Siemens PLM Software