Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - Maintenance Pack 9 Announcement

Siemens Legend Siemens Legend
Siemens Legend

August 8, 2017

 

Dear Solid Edge Customer:

  

Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 9 is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and

installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked

as Installed Updates.

 

=============

Update Version:

=============

 

109.00.09.05

 

================

Download Location:

================

 

ST9 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be

uninstalled using Uninstall a program from the Control Panel.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update

  with a lesser version.

 

  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered

  in MP1 and MP2.

 

  • MSI Product Updates calculate free disk space before installing. Please note that there have

  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.

 

  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.

 

  • Uninstalling a MSI Product Update will restore the installation to the state before the Product

  Update was applied.

 

  • PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous

  Product Update package, if any, must be available to allow the recovery of previous file versions.

 

  • The current MSI Product Update will be the only Update listed and available for uninstallation.

  After the current Update is uninstalled, the previous Update will become the current Update, if

  there were multiple Updates installed.

 

  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed

  updates -> Uninstall).

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail

notification.

 

For details on initiating your email subscription navigate to:

http://support.industrysoftware.automation.siemens.com/general/email.shtml

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Part/Profile/Sheet Metal===

PR 8890108: Error observed when 'Dynamically Preview ...' is unchecked.

PR 8892876: Impossible to trim framing Simulation geometry.

PR 8897967: Hidden PMI Dimensions detached after edit

PR 8897575: Save as flat as DXF causes an open contour in the DXF file

PR 8919490: Status message not shown while physical properties are being updated

 

===Assembly===

PR 7953538: Improved performance with enumerating sub-occurrences.

PR 8839129: Standard Parts Dialog Display Clipped at 4K Resolution

PR 8897746: Recognize appropriate size of reducer by standard parts

PR 7587050: Peer edge locate does not work for a specific arc of an assembly component

PR 8889402: Solid Edge crash when opening the supplied assembly

PR 8916330: Assembly will not open for customer

PR 8862802: Additional relations result in failed relations in specificasm

PR 8917774: Abort in Assembly when updating documents

PR 8925555: Abort at GStrip::GetSize when opening an assembly.

PR 8926386: Draft not showing assembly generated item numbers when the item number mode is top-level only.

PR 8889695: Assemblies only will not open in Solid Edge ST9, MP7, Win 8?

PR 8919490: Status message not shown while physical properties are being updated

PR 8920421: Fixed a crash found via Crashlog Analysis.

                                                                                                                                                          

===Draft===

PR 8825442: some fills/annotations/dims on drawing views changing on open when model not present.

PR 8829050: Problem with batch program not running all files in folder using convert to

PR 7977163: 2D Model View not placed at the lower left hand corner of the Draft Sheet

PR 8929818: Double clicking on a drawing view lead to an abort - not reproducible.

PR 7856119: Not getting a blinking cursor when editing dimensions

 

===Translators===

PR 8844252: false JT-Export options in german (non-english) version

PR 8900746: Conversion from Solidworks to Solid Edge had been terminated

PR 8918420: SW data Migration of a draft terminates at dxf creation point.

 

===API===

PR 8826955: FaceStyle() return incorrect object as well as SkyboxClearAll() does not clears

 

===General===

PR 8896473: Solid Edge crashes when opening par file. Please repair in ST9

PR 8918661: 1000s of errors displayed in Event Viewer - source SENativePDM cannot be found

 

===Teamcenter Integration for Solid Edge===

PR 8324141: Extend existing parts in TC managed mode doesn't allow to add new part

PR 8900636: Data Prep commands in the xls not working on Windows 10 1703.

PR 8867425: SEEC Solid Edge crashes on save event (Draft).

PR 8891128: Add to Teamcenter - fails to load any files with a Solid Edge crash

PR 8919539: Duplicate Structure via Structure Editor does not give expected result

PR 8924229: SEEC_BOM_Synchronize is losing non-saved driven references

PR 8828094: jt overrides not uploaded if 2 assemblies on CPD

PR 8927624: SEEC BOM Synchronize does not recognize component that is a SE Assembly.

PR 8898826: SEEC crashed after working on large ASM for long time and close the file

 

===Solid Edge SharePoint===

PR 8333022: Double quantity of all parts in Relation Browser & BOM report from

 

===Built-in Data Management===

PR 8918150: Solid Edge ST9 MP08 breaks Fast Search

 

===Design Manager===

PR 7974034: Can't do a Save As on released files without DocControl permissions

PR 8940176: Unable to create a new revision of an assembly using Design Manager

PR 8341431: Replace (Find/Replace) should have an option to use Actions files only

PR 8922239: Perform Release action shows warning & action don't complete

PR 8924027: Clear action do not update SE Status for multi-bodies.

PR 8896339: Assembly with part - Ctrl+S breaks the link

PR 8885083: Save As action to assembly with FOP members breaks the FOP links

 

Regards,
Fred White
Siemens PLM Software
1 REPLY

Re: Solid Edge ST9 - Maintenance Pack 9 Announcement

Phenom
Phenom

Hi @JFred

 

thanks,

 

Arek


Production: SE ST10 MP8
;