Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 - New tools

Hi all,

 

this week I have started with ST9, looks amazing. The GUI is very good.

Love several new and fine-tuned tools.

 

I have a question about the Drafting highlights - Dimensions and annotations

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:index#goto:newse:xid667374

Where can I find the Hole callouts with shown hole count?

I just cannot find it.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
2 REPLIES 2

Re: Solid Edge ST9 - New tools

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is no button for it.  If you would have drilled a little further in the Help you would have gotten here: https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:index_newse:xid459404:xid1151068

 

In the Smart Depth section of the Callout Properties you will see a new Hole Quantity Note section.  If using the default ST9 templates, it will be filled in with "%QC X".  Also, if you invoke the Select Symbols and Values form, expand Values and then Feature References, you will find three of the new Quantity codes.

 

According to the Property Text Codes Help page, there is also a %QN code for a smart Quantity:  https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:index_annotations:xid280274:symtxt1...

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST9 - New tools

Hi,

Thanks
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10