Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 opening STL wrong dimensions

Experimenter
Experimenter

I'm running Solid Edge ST9 MP3 and when I create object and save it as STL file units in mm and open the same file the units are opened as inches, so model is 24,5 times bigger (units in the model are still mm but object is 24,5x bigger).   It's not a problem of system units, they are set to MMKS.
The file is saved correctly cause under NX the dimensions are as they should be.

Anyone have same issue?

STL units.pngSTL settingsUnits.pngSolid Edge system units

2 REPLIES

Re: Solid Edge ST9 opening STL wrong dimensions

Legend
Legend

Take a look at the options befor import. If you choose "mm" there, it works like a charme.

Greetings from Germany
Christian Kunkel
https://c-k-m.info

Re: Solid Edge ST9 opening STL wrong dimensions

Experimenter
Experimenter

Thanks, didin't notice the Options in the menu there.