Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge - STEP 24and PMI import/export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,

 

 

reagrding to the STEP 242 definition and what I have seen so far from other CAD software, the PMI objects should be usable for STEP exchange to other CAD/CAM/CAQ software packages.

 

I have seen working STEP exports with PMI from NX but importing them into SE will leave all PMIs away.

Same is true for a direct NX part import with PMI objects, they are not imported too.

 

Do I miss any setting or option or is it a "sorry we don't support it!" issue.

 

 

regards
Wolfgang
2 REPLIES 2

Re: Solid Edge - STEP 24and PMI import/export

Gears Phenom Gears Phenom
Gears Phenom

Smiley Sad Unfortunately the 2nd one... "we don't...". Other thing is that Solid Edge doesn't support at exporting & importing file attributes or metadata, so we have only a body without titel, material, and others...

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge - STEP 24and PMI import/export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

 

 

Not really thats answer I hoped to get, but at least the confirmation of what I feared to be the current fact.

 

Hi Solid Edge Developers, this ist something wehre wenn Need improvements sono.

 

 

regards
Wolfgang