Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Simulation Bolt Loads

Is it possbile to query bolt tensile and shear loads from bolts created using the Solid Edge Simulation bolt assembly connector?

 

bolt_loads.jpg

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
3 REPLIES 3

Re: Solid Edge Simulation Bolt Loads

Honored Contributor
Honored Contributor

Bolt group loads are a can of worms. Best to consult AISC.

 

I can't take any responcibility for accuracy or any persons ability to the the attachment. I have found the attached spreadsheets to be valuble for some basic calculations including bolt groups.

 

 

Re: Solid Edge Simulation Bolt Loads

Siemens Phenom Siemens Phenom
Siemens Phenom

David,

as far as I know you can't plot the Bolt Beam Element Vectors, like in Femap for example.

Altough Femap is the "motor" in SE Simulation.

 

You may log something on this to your VAR.

 

/Ulf

Siemens EMEA GTAC Support
Highlighted

Re: Solid Edge Simulation Bolt Loads

Thanks, this was also confirmed via GTAC email. They said there was an existing enhancement request to add a feature to display bolt reaction loads.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10