Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Simulation - combination of beam and plates

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Solid Edge Analysts,

From the quick observe of the Solid Edge simulation it is probably not possible to analyze frame with sheets, e.g. frame structure with some reinforcement plates in corners. If I run the simulation within active frame I can generate only 1D mesh. If I am out of frame in assembly, it is possible to generate shell elements on plates, but no possiblity to generate 1D mesh.

Is this somehow possible? Some workaround?

Juraj

1 REPLY

Re: Solid Edge Simulation - combination of beam and plates

Gears Phenom Gears Phenom
Gears Phenom
Hi,

There is no way to do what you want. Only way is building a simulation geometry via shell elements (surface copy & offset them).

BR,
Imics
http://solidedgest.wordpress.com/