Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge St8 Install Error

Experimenter
Experimenter

We have a customer who is switching to SESt8 and one of our computers errors out on the install at the very end.

 

What is the possible fix?  There is nothing that we (IT) can find "wrong" on this computer.

 

We have tried (and it is no fast process) to download the Program and install it to no avail.

 

Would we be able to "copy" it from another computer and use it?

1 REPLY 1

Re: Solid Edge St8 Install Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Was the previous version uninstalled?

Was the PC restarted after the uninstall?

Was the install file right clicked on and the option to "Run as Adminstrator" selected?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com