Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Stencil

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I noticed doing a text profile on the capital letter M. There are two lines intersect one and another.

The text is under Solid Edge Stencil. Is this an error in Solid Edge Student Edition? or can I fix!

 

http://screencast.com/t/BqNkqx49A7Z

 

Thank You

Greg

4 REPLIES

Re: Solid Edge Stencil

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not seeing it.  Looks fine for me.  Post what your text profile parameters are and I will try and reproduce.

m.png



Ken

Production: ST10 MP6
Testing: SE 2019

Re: Solid Edge Stencil

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I see the same result as Ken,....as he say's, can you provide your text profile attributes?, as there may be a clue there.

 

SE_Sketch_TextProfile_SolidEdgeStencil_Attributes.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Solid Edge Stencil

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

This parameter may help with the capital letter M.

 

http://screencast.com/t/N2k7Z38jM5

 

Thank You

Greg

Re: Solid Edge Stencil

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's the "Bold" parameter that is causing it.  Turn off Bold and then it works fine.  This setting shouldn't be used with the stencil font as the amount that it thickens it is negligible, and as you have seen, causes overlapping geometry.  I am still going to log it as an issue though...



Ken

Production: ST10 MP6
Testing: SE 2019