Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid Edge Translation Services

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,



just tried the SOlid Edge Translation Sevies .exe to use it for automized translation (export) of Solid Edge data.

 

According to the info and help found under:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/Translating-Solid-Edge-Files-from-th...

 

 

I always get an error message back with no success in translation.

 

Can anybody confirm this with ST9 wether this generally doesn't work or wether I have a problem here with this local installation.

 

Thanks in advance

 

 

 

BTW: I thought to rmemeber an extra program to import/export Solid Edge files to parasolid.

But I don't find it.

Is this also a piece of tools taken away with one of the last versions or again a problem of

"The Old men with the Bad Eyes"

 

regards
Wolfgang
7 REPLIES 7

Re: Solid Edge Translation Services

Gears Phenom Gears Phenom
Gears Phenom

Solid Edge ST9\Custom\Batch\Bin\batch


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Solid Edge Translation Services

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Johnson_BigMatt

 

 

thanks.

The Batch macro was in my mind but I thought there was - and now I got the confirmation from another source that thee was an external translator in the program folder to import/export from/to parasolid which seems to be canceld/take out for supoose 2 versions now.

Same happend with the STEP translator, but here I can understand the changes due to the changes in step translator.

 

 

If it would be possible to use these new Solid Edge Translation Services Exe instead, then OK, but they don't seem to work properly.

At least at the moment forme.

 

PS.: the idea should be a "batch" translation without the need of staring Solid Edge itself, what was possible using the translator tools.

 

regards
Wolfgang

Re: Solid Edge Translation Services

Gears Phenom Gears Phenom
Gears Phenom

@hawcad   Agreed!

 

Dont forget... there is a whole new world out there within the API!!!

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Solid Edge Translation Services

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Johnson_BigMatt

 

 

 

of course there is "this" hole new world outside, but is it a must to enter it? Robot wink

 

There already were  working tools vailable for years and for many many versions.

And then they are suddenly taken away, with now uderstandable reason.

 

Of course we can try to create a macro but this also might would mean to - somehow - strat Solid Edge i the back, running it for a task which - as it seems - should be heer and working.

 

I hope to hear froom support and development, how it could be solved and why it doesn't work yet.

 

But also, thanks for Your efforts @Johnson_BigMatt

 

 

regards
Wolfgang

Re: Solid Edge Translation Services

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad SolidEdgeTranslationServices.exe just automates Solid Edge to do the translation invisibly.  You would need to make sure you can successfully save out the file type manually which will insure your options are set correctly.  Once that is done, SolidEdgeTranslationServices.exe should work...  It is working for me to save PDF's from Draft files.

 

path\SolidEdgeTranslationServices.exe -i="input file path and name" -o="output file path and name" -t=filetype (PDF, IGS, STP, DWG)



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge Translation Services

Siemens Phenom Siemens Phenom
Siemens Phenom

As the author of the blog post referenced, I can also confirm that the SolidEdgeTranslationServices.exe is working as expected in ST9.  

 

EDIT:  Also, you will need to provide the full path for both the input and output file names.

Re: Solid Edge Translation Services

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

thanks for that info, which I just got from Kay too.

 

the hint with the "Full Pathname" was it.

 

I never thought that this could be necessary, and therefore always used relative names instead.

 

 

regards
Wolfgang