Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Video Recording Setting for Area

Gears Phenom Gears Phenom
Gears Phenom

I tried digging in the registry but could not locate a setting to have the following setting by default.

  

SERecordScreen.png

  

Fortunately it is required to be set only once for a session and not with every new document. Still I would prefer the whole SE screen and not just the active document to default for recording every time I start Solid Edge.

 

~Tushar

5 REPLIES

Betreff: Solid Edge Video Recording Setting for Area

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

 

Yes this is something what annoys me too everytime when recording a SE video

 

This would be a big enhancement

 



regards
Wolfgang

Betreff: Solid Edge Video Recording Setting for Area

Honored Contributor
Honored Contributor

I want the entire desktop. That is not an option either. I use two screen, with variables open on the second monitor. Also I have windows file there to be dragged in. I made a few movies for GTAC last night and thought there was a way to get the entire desktop. I could get close with an area across both screens, but that's still not the same thing.

Betreff: Solid Edge Video Recording Setting for Area

Gears Phenom Gears Phenom
Gears Phenom

Guys, go slow on the kudos, I have simply asked a question.

Betreff: Solid Edge Video Recording Setting for Area

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

 

but the right question at the best time!

 

Smiley Happy

 

 

As I say someties:

 

"It is not enough to be irritated about something,

and to keep still about,

You also have to claim a change and
You have to make suggestions how to improve it!"

 

Then, things will change!

 



regards
Wolfgang

Betreff: Solid Edge Video Recording Setting for Area

Valued Contributor
Valued Contributor

Hello everyone ..
Most of the edges are based on values that are not frequently used by default.
This will vary from user to user, but it must be changed to allow setting for each user.
In other words, you should be able to save the defaults as you like.
This part is very disappointing.