Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Viewer Not Allowing Sections

Experimenter
Experimenter

Hi All,

 

I've downloaded the latest version of the SE viewer but it won't allow me to take sections or mark-up the model. All the buttons are greyed out.

 

Am I missing something?

 

Thanks/

3 REPLIES

Re: Solid Edge Viewer Not Allowing Sections

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have never had the need to use it......but, did the viewer ever allow you to do this?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Solid Edge Viewer Not Allowing Sections

Genius
Genius

Hi,

 

Markup, measurement and section in SE Viewer works only for .pcf files. Not for SE native .par .psm and .asm files.

 

There is a paid version of SE Viewer called View and Markup. It comes bundled with Solid Edge and can also be bought separately. The idea is that the engineer opens an assembly in V&M and saves it as a single .pcf (packed collaboration) file for review purposes. He can send the .pcf to anyone with SE Viewer installed, without giving away the entire design.

 

Robin.

Re: Solid Edge Viewer Not Allowing Sections

Gears Phenom Gears Phenom
Gears Phenom
Hi,

What was mentioned by @vongahlen is correct for ST7, but you can use measurement in ST8 viewer on native SE files. Unfortunately section is not allowed in it, but I don't understand why?
Anybody from developers? 😎

Best,
Imics
http://solidedgest.wordpress.com/