Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Viewer for I phone

Valued Contributor
Valued Contributor

Is there a solid edge viewer for the I-phone? I know there is one for the I-pad.

 

For the solid edge viewer it would also be nice to pull PMI dimensions. You can have the option when saving a .sev file to enable measuring or not.

 

Thank you

5 REPLIES 5

Re: Solid Edge Viewer for I phone

Phenom
Phenom

ALthough, the iPhone and iPad share the same OS I don't think this will work on the the iPhone due to the UI. I'm hoping that I am wrong here but I don't think I am.

https://itunes.apple.com/us/app/solid-edge-mobile-viewer/id527999141?mt=8

Re: Solid Edge Viewer for I phone

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Solid Edge viewer doesn't work on Iphone only on Ipad, If I remember well.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge Viewer for I phone

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I suggest using 3D pdf with PMI, this works well.

 

Here is an app from iTunes. I use it on Ipad & Iphone too.

https://itunes.apple.com/us/app/3d-pdf-reader/id569307672?mt=8

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge Viewer for I phone

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imics wrote:

Hi,

 

I suggest using 3D pdf with PMI, this works well.

 

Here is an app from iTunes. I use it on Ipad & Iphone too.

https://itunes.apple.com/us/app/3d-pdf-reader/id569307672?mt=8

 

BR,


 

I have that same app, but the Android version.....it works well.

Not sure why the SE-Viewer doesn't have the option to install on iPhone.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP6] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge Viewer for I phone

Valued Contributor
Valued Contributor

One of the main reasons I am bringing it up is to maybe get a few enhancements done to the mobile viewer.

 

There is an app for the I-Pad, why not the I-phone.

 

Other enhancements I would like to see would be:

 

1) When saving the .sev file have the option to give permission to the recipient to measure the model and comment on the model.

 

2) The person opening the .sev file is able to comment and save the file and send back to the originator of the .sev file or other team members.

 

3) Some mobile devices are limited for display space but to have a display of the model tree where you can show and hide components by clicking on a check box similar to the assembly environment of solid edge.

 

4) Since many of today's printers have wifi connection, the ability to connect to a printer and print the current screen image of a model or if a .sev of a draft was created, print the mfg drawing.

 

Just a few thoughts to share