Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge can not open

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I can not open my Solid Edge, when I open just show Server Busy as picture shown bellow

I tried to uninstall and install again but can not solve

Please help us to solve this prolem

Solid Edge can not open.jpg

5 REPLIES 5

Re: Solid Edge can not open

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I click the Switch To button normally when this prompt appears and Solid Edge is then visible on the screen, although I don't know why this happens.

 

Re: Solid Edge can not open

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I tried to click Switch many time but can not changed

Re: Solid Edge can not open

Valued Contributor
Valued Contributor
I would guess you are best doing a full uninstall, then remove any registry entries as well as residual program folders. Reinstall (run as admin) and disable you anti-virus while doing so.


CAD/CAE Manager
ST8 MP9

Re: Solid Edge can not open

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you happen to also install the Solid Edge Viewer?  The 2 are not supposed to be installed on the same PC and doing so will break the Solid Edge installation.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Solid Edge can not open

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Thanks for your help! Maybe one problem relevent to MS office When i uninstall and reinstall MS office, after that I open Solid Edge running nomally