Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge can save dft as pdf. But pdf has not any component.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi!

 

 

My customer saved Solid Edge Draft file as pdf file.

But created pdf file has not any components.

Pdf file shows background only.

 

What's wrong with my customer's system?

 

Please let me know.

 

 

Thank you!

18 REPLIES 18

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @LittleWillie76

 

 

 

which Solid Edge version, Maintenance Pack and Operating system is in use?

 

regards
Wolfgang

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi, Mr. Wolfgang.

 

 

Thanks to your attention to my issue.

 

Solid Edge version is ST9 and MP8... and Windows 7 64bit...

 

 

Best Regards

LittleWillie

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

And Korean version

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Siemens Phenom Siemens Phenom
Siemens Phenom

Is the user using the Save As or Save As Translated to create the PDF?  Or is the customer printing the file to a PDF printer?  Depending on which path is used to generate the PDF file this may then impact the behaviour.

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi, uk_dave!

 

 

Executed 'Save As' command on draft mode.

 

How does the path affect to behaviour?

 

For example, path is too long or path contains some special characters?

 

 

Best Regards

LittleWillie76

Re: Solid Edge can save dft as pdf. But pdf has not any component.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Difficult to tell without looking at the Solid Edge Draft file.

Please attach it here if possible.

  

In the Save As dialog is the Options... button, have you tried tweaking some setting in there ?

 

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Siemens Phenom Siemens Phenom
Siemens Phenom

Path as in the "steps taken to create the PDF file" not path as in the "filename". 

 

I can rewrite that sentence as "Depending on which method is used to generate the PDF file this may then impact the behaviour." If that helps.

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Siemens Phenom Siemens Phenom
Siemens Phenom

When doing the Save As to PDF, under the Options is the "Sheet Options" set to "All sheets"?

Betreff: Solid Edge can save dft as pdf. But pdf has not any component.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Selected "Activated sheet only"...