Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge can use in Maya software?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi there;

I need to save the model from Solid Edge to Maya. Is this possible? What formats can Solid Edge export?

 

Thank.

5 REPLIES 5

Betreff: Solid Edge can use in Maya software?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Famer

 

 

 

sorry for not knowing Maya taht much, but the IMHO more important questionis:

 

"Which formats is Maya able to read in?"

 

Normally they should be able to read those standard neutral formats like Parasolid, Step, or some othes.

 

 

regards
Wolfgang

Betreff: Solid Edge can use in Maya software?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Now.They use Illustrator import Iges files form 3D CAD and save to AI file to use in Maya software.

Re: Solid Edge can use in Maya software?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

As mentioned by @hawcad, you need to check the list of formats that Maya can import against those Solid Edge can export to get the best combination working for you. Sometime there could be issues with the way one pair of formats will import Solid Edge data into Maya.

 

Also attached is an Excel file with a handy list of import/export options for various software for easy reference. Hope you find it useful.

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

[ Everything under the sun about - Solid Edge ]

Re: Solid Edge can use in Maya software?

Phenom
Phenom

I had pretty good results using JT format to export from Solid Edge to 3dsMax without 3rd party software - perhaps that's something you could try for Maya.

Re: Solid Edge can use in Maya software?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you so much for imformation.