Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid Edge certification exam

Experimenter
Experimenter

Hi, I am a university student and I have to take the Solid Edge certification exam as part of my university program. But I am unsure on how to enter the answers in the certification, I know I can only enter numeric values and no commas ','. But what if I get a distance value of 123.64mm in Solid Edge, do I have to enter 123.64 or 124 or 12364?

2 REPLIES 2

Re: Solid Edge certification exam

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Set the unit precision to zero when taking the exam.

This will take care of the rounding automatically.

The setting is under the Solid Edge Application button - Options - Units tab.