Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge closes every time I try to start a new part etc

Experimenter
Experimenter

Solid Edge ST7 installed with no problems at all during installation yet everytime I try to do something like start a new part it just completely closes down. I looked in task manager after this happened but no processes appear there. Also tried oppening existing parts with the same result. Uninstalling and reinstalling did not help either. Apologies if this is the wrong place for this, wasn't sure where to post.  

 

Help much appreciated!  

10 REPLIES

Re: Solid Edge closes every time I try to start a new part etc

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
What operating system are you using?
Mark

Re: Solid Edge closes every time I try to start a new part etc

Experimenter
Experimenter
Hi, I'm using Windows 7 64 bit.

Re: Solid Edge closes every time I try to start a new part etc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Possibilities could be a bad install or a corrupted registry.  You might try uninstalling and performing a SECleanUpAll (found in the download under a folder called SptTools) and then reinstall.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Solid Edge closes every time I try to start a new part etc

Experimenter
Experimenter
Thanks for the suggestion, sadly the same problem still exits after carrying out the clean and re downloading the solid edge install

Re: Solid Edge closes every time I try to start a new part etc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So the corrupted registry thing is a bit harder to fix.  You have to use REGEDIT to do this and if you delete the wrong thing you can mess up your PC to the point it may need to have the OS reinstalled, so be carefull!

 

Deleting the following key will remove all of your registry settings for Solid Edge: HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge

 



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Solid Edge closes every time I try to start a new part etc

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you can start a new Draft document but not a part or assembly I would look at 3D graphics settings.

If this is the case try updating your graphics driver.

There is a text file that will auto-select the settings based on your card.

"C:\Program Files\Solid Edge ST7\Program\AutoConfigure.txt"

LMGi
www.TLMGi.com

Re: Solid Edge closes every time I try to start a new part etc

Experimenter
Experimenter
I uninstalled, deleted the registry edit then reinstalled all to no avail. Draft documents won't work either it seems.

Re: Solid Edge closes every time I try to start a new part etc

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Did you turn of user account control UAC?

 

Re: Solid Edge closes every time I try to start a new part etc

Experimenter
Experimenter
As far as I can see UAC is just on the default setting.