Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge crash when opening an .par file

Experimenter
Experimenter

When I open a new Isometric Part or want to change on, the Program crashes. A few days ago everything was ok and i could do what i want, bur now I cant open Isometric Parts. 

1 REPLY 1

Re: Solid Edge crash when opening an .par file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It appears the crash is a result of the open gl driver from the NVIDIA driver update.  You should revert back to the older driver if that worked.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com