Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge drafts - Can I change the style for all objects quickly?

Valued Contributor
Valued Contributor

Hi,

 

Is there a quick way to change the style of all objects in a draft (dims, text, tables etc)?  Beyond that is there a batch process that could do this?

 

The reason I ask is we have our own company styles setup stored in the template.  I've discovered a number of drawings that have been done using the wrong style and would like to change them en masse if possible?

 

At the moment I'm telling the users to use smartselect to pick all similar elements then change the style via the dropdown menu.

 

Thanks for any help,

Guy


CAD/CAE Manager
ST8 MP12
6 REPLIES 6

Betreff: Solid Edge drafts - Can I change the style for all objects quickly?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Guy_H77

 

 

 

does a change of the format styles help?

 

Reimporting the fomrta styles from new template or MTL should define all objects which was created using that style.

 

I think that there is a batch program which will do this too.

Not absoluteley confident wether the "Change_Background" or the "OpenSave" will do this at them moment.

 

 

regards
Wolfgang

Re: Solid Edge drafts - Can I change the style for all objects quickly?

Honored Contributor
Honored Contributor

I have found is that the styles are associated witht the file, not the install. So if the styles are not already in the files, they have to be created. For details styles it goes even a step further. You have to open a template, use some model on it so that details can be added to the draft, develope and save the styles, then delete the model used before saving it back to the template.

 

The good news is that the text selection and size will control just about everything except detail styles.

Re: Solid Edge drafts - Can I change the style for all objects quickly?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @12GAGE

 

 

You can save the format styles into the material database files too.

So from any drawing You have in use and where the proper style is available You can store it back into the Material.MTL and vice versa

 

regards
Wolfgang

Re: Solid Edge drafts - Can I change the style for all objects quickly?

Honored Contributor
Honored Contributor

What is the procedure for that? I don't understand how say, the style for view details can be saved and recalled from the material database.

Re: Solid Edge drafts - Can I change the style for all objects quickly?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @12GAGE

 

 

maybe we are talking about different things at the moment.

So let's clarify.

 

When I talk about styles - and so I understood the original question - I think about dimensions styles, text styles etc.

 

And those format styles could be saved either in a Solid Edge file like draft, part, etc but also - and fo rme this seems to be the default - in the material datebase file.

This is a centralized file for several Solid Edge formats definitions.

Colors, hatch, line types, text styles, dim styles etc.

As a matter of fact this file is used more or less at any time and mostly is saved at the server, it also offers to be used as storage for this things.

And from there You can get it or to that location You can send it.

 

Is this You are takling too?

 

 

regards
Wolfgang

Re: Solid Edge drafts - Can I change the style for all objects quickly?

Valued Contributor
Valued Contributor

Just wanna add that you have to take care when you copy any style to the MTL database, since there are styles that are different between type of documents but they share same name (ISO or ANSY), I mean you have your dimension styles in your MTL database and in my case those are the styles present in PAR and ASM files but the style I use on my drafts are diferent (they share same name, company name in my case), If I copy or transfer my dimension style from the draft to the MTL database I´m overriding styles used in par and asm, so you have to rename the style.