Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge to *.NC file

Has anyone have any success in exporting *.NC files from Solid Edge?

 

An *.NC file, is kind of a 3D DXF file that is used for processing structural steel beams.

The file contains data including: Beam Size; Beam Length; Hole Dia / Qty / Locations etc.

Using the *.NC file on a 'Beam Line' (a CNC machine for structural beams) automates the beam process that it is ready for fabrication.

 

We have been looking at this for a number of years, with only limited success of finding any solutions.

In recent months, it has become apparant that most of the steel suppliers have moved to the Beam Line machinery, and really need the *.NC file to be able to process the steel.

 

The main Steel Detailing type CAD softwares like Tekla; ProSteel etc. can generate a *.NC file direct.

 

For other softwares, a 3rd party add in is required.

I have in the past found add-ins for softwares including Solidworks; ProE; and Inventor, but very little in regards to Solid Edge. I have contacted many of these, who showed little interest in adapting their software to suit an alternate CAD.

 

The only company that i have found that seems to acknowledge Solid Edge, is Klietsch in Germany ( www.klietsch.com )

 

So my questions are:

- Is anyone successfully exporting NC data from SE, and if so how?

- Are there other SE users that would value the NC export tool?

 

David

 

David Finlay
7 REPLIES 7

Re: Solid Edge to *.NC file

Re: Solid Edge to *.NC file

Phenom
Phenom

We export STEP files to send to our sub-contract fabricators who then can import this into their CAM sofware to create NC files - the process you describe is approximatly the same as programming for 2D laser profiler, 3D tube laser or CNC mill.

 

You'll probably find more luck in searching for standalone CAM software that can import neutral files, rather than finding a plugin to solid edge which are few and far between compared to some of the competition.

Re: Solid Edge to *.NC file

Experimenter
Experimenter

Hiya David,

 

 

I have to provide NC files when I produce a drawing / fabrication pack for my customers. After trying a few options out and trialing different softwares I now get a company to convert my files.

 

I send them 3D step files and they send me back NC files. They are super quick and ive not had a problem in the past. The bonus is that i dont have to worry about sorting them myself!

 

NcDSTV@gmail.com - The are called NC Solutions. 

 

 

Re: Solid Edge to *.NC file

Legend
Legend

Hi,

 

Is there any news around this subject, would like to make NC or DSTV files from our Solid Edge steel constructions.

 

Reg.

 

Jan Bos

Emmen, The Netherlands

Solid Edge user since V3.5 beta testing ST10

 

Re: Solid Edge to *.NC file

Experimenter
Experimenter

Hi,

I also have a need to be able to export NC1 files from Solid Edge. I have sought assistance from SE support but to date have had little response othe than - Yes we should investigate,

Selwyn.

Re: Solid Edge to *.NC file

Siemens Phenom Siemens Phenom
Siemens Phenom

@Selwyn currently Solid Edge cannot export to the DSTV or NC file format.  There is master ER# 1373377 tracking this request.

 

Aside from you asking your local Solid Edge support to attach your sold-to id to this existing master ER I am not sure what else you are expecting from support when currently the software does not offer this functionality.


The user @CADCAM1 has kindly posted above a company that will help you create these files.  That service's website is https://nc1-solutions.com/

 

If you wish to PM your contact details and sold-to id I can certainly investigate further as to why you seem to be getting little response to this from Solid Edge support.

Re: Solid Edge to *.NC file

Legend
Legend

We have used contractors to convert solid edge steps to NC.. they use Tekla..

 

We have a lot of examples now how the NC code is done..

 

Its just a simple textfile that can be edited with notepad or better notepad++

 

Simple parts that need updating is now done via an edit to the text, than opened in an viewer, and if needed exported to Step and imported into Solid Edge for checking..

 

The viewer that also can export to step can be downloaded from

http://www.hgg-group.com/nl/knowledge-base/hggs-free-dstv-viewer/

 

The code looks like

 

ST
** NTVW1806d.nc1
  NTVW1806d
  L80/40
  8
  L80/40
  S235JR
  -
  L80/40/8
  L
    420,420.00
       80.00
       40.00
        8.00
        8.00
        7.00
        7.07
        0.230
        0.000
        0.000
        0.000
        0.000




AK
  v       0.00u      0.00       0.00       0.00       0.00       0.00       0.00
        420.00       0.00       0.00       0.00       0.00       0.00       0.00
        420.00      80.00       0.00       0.00       0.00       0.00       0.00
          0.00      80.00       0.00       0.00       0.00       0.00       0.00
          0.00       0.00       0.00       0.00       0.00       0.00       0.00
AK
  u       0.00o      0.00       0.00       0.00       0.00       0.00       0.00
        420.00       0.00       0.00       0.00       0.00       0.00       0.00
        420.00      40.00       0.00       0.00       0.00       0.00       0.00
          0.00      40.00       0.00       0.00       0.00       0.00       0.00
          0.00       0.00       0.00       0.00       0.00       0.00       0.00

BO
  v      35.00u     45.00      26.00
  v     385.00u     45.00      26.00

EN

 

Viewed in the viewer

NC code omschrijving.jpg

Would be nice if Solid edge could export  and import NC files.

 

Kind Regards,

 

 

Jan Bos

Emmen, The Netherland

Solid Edge user since V3.5, Beta testing ST11